Part Number: AM5708
Please check the below log and suggest us how to proceed further.
Build Log:->
:~/bwt/tisdk/build$ TOOLCHAIN_PATH_ARMV7=$HOME/gcc-arm-8.3-2019.03-x86_64-arm-linux-gnueabihf MACHINE=am57xx-hs-evm bitbake core-image-minimal
WARNING: Layer meta-processor-sdk should set LAYERSERIES_COMPAT_meta-processor-sdk in its conf/layer.conf file to list the core layer names it is compatible with.
WARNING: Layer meta-processor-sdk should set LAYERSERIES_COMPAT_meta-processor-sdk in its conf/layer.conf file to list the core layer names it is compatible with.
Loading cache: 100% |########################################################################################################################################################################| Time: 0:00:00
Loaded 4658 entries from dependency cache.
WARNING: No recipes available for:
/home/user/bwt/tisdk/sources/meta-arago/meta-arago-distro/recipes-browser/chromium/chromium-wayland_%.bbappend
/home/user/bwt/tisdk/sources/meta-processor-sdk/recipes-ros/navigation/move-base_1.12.14.bbappend
/home/user/bwt/tisdk/sources/meta-processor-sdk/recipes-ros/navigation/rotate-recovery_1.12.14.bbappend
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION = "1.40.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-18.04"
TARGET_SYS = "arm-linux-gnueabi"
MACHINE = "am57xx-hs-evm"
DISTRO = "arago"
DISTRO_VERSION = "2019.11"
TUNE_FEATURES = "arm armv7a vfp thumb neon callconvention-hard"
TARGET_FPU = "hard"
meta-processor-sdk = "HEAD:56d9d47f18eeec31a1086ca29e54b5956c46de84"
meta-aws = "HEAD:6432f1b38b9dcbbb55020167f5b1cfe55e858c6d"
meta-ros = "HEAD:72068b17e4192b51e09c8dc633805a35edac8701"
meta-arago-distro
meta-arago-extras = "HEAD:70436496d2617b281c51390faa3d421814055cd6"
meta-browser = "HEAD:5f365ef0f842ba4651efe88787cf9c63bc8b6cb3"
meta-qt5 = "HEAD:e6e464c9ed9266ce46452f953c1bdcb0e7b2d95f"
meta-virtualization = "HEAD:7685c7d415e0002c448007960837ae8898cd57a5"
meta-networking
meta-python
meta-oe
meta-gnome
meta-multimedia
meta-filesystems = "HEAD:446bd615fd7cb9bc7a159fe5c2019ed08d1a7a93"
meta-ti = "HEAD:b27317ab4f9be931a66344ca502c7e3f4ec780e5"
meta-linaro-toolchain
meta-optee = "HEAD:615ea7561b844a3867cee4299d83d605c10b02ab"
meta = "HEAD:e68991ceb5933f7d03b96697e8a0ba0829feb320"
Initialising tasks: 100% |###################################################################################################################################################################| Time: 0:00:03
Sstate summary: Wanted 144 Found 0 Missed 144 Current 410 (0% match, 74% complete)
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: linux-ti-staging-4.19.94+gitAUTOINC+be5389fd85-r7a.arago5.tisdk1.1 do_assemble_fitimage: Function failed: do_assemble_fitimage (log file is located at /home/user/bwt/tisdk/build/arago-tmp-external-arm-toolchain/work/am57xx_hs_evm-linux-gnueabi/linux-ti-staging/4.19.94+gitAUTOINC+be5389fd85-r7a.arago5.tisdk1.1/temp/log.do_assemble_fitimage.16431)
ERROR: Logfile of failure stored in: /home/user/bwt/tisdk/build/arago-tmp-external-arm-toolchain/work/am57xx_hs_evm-linux-gnueabi/linux-ti-staging/4.19.94+gitAUTOINC+be5389fd85-r7a.arago5.tisdk1.1/temp/log.do_assemble_fitimage.16431
Log data follows:
| DEBUG: Executing shell function do_assemble_fitimage
| none
| /home/user/bwt/tisdk/build/arago-tmp-external-arm-toolchain/work/am57xx_hs_evm-linux-gnueabi/linux-ti-staging/4.19.94+gitAUTOINC+be5389fd85-r7a.arago5.tisdk1.1/temp/run.do_assemble_fitimage.16431: line 569: /am5x/scripts/secure-binary-image.sh: No such file or directory
| WARNING: /home/user/bwt/tisdk/build/arago-tmp-external-arm-toolchain/work/am57xx_hs_evm-linux-gnueabi/linux-ti-staging/4.19.94+gitAUTOINC+be5389fd85-r7a.arago5.tisdk1.1/temp/run.do_assemble_fitimage.16431:1 exit 127 from '${TI_SECURE_DEV_PKG_AUTO}/am5x/scripts/secure-binary-image.sh $1 $2'
| ERROR: Function failed: do_assemble_fitimage (log file is located at /home/user/bwt/tisdk/build/arago-tmp-external-arm-toolchain/work/am57xx_hs_evm-linux-gnueabi/linux-ti-staging/4.19.94+gitAUTOINC+be5389fd85-r7a.arago5.tisdk1.1/temp/log.do_assemble_fitimage.16431)
ERROR: Task (/home/user/bwt/tisdk/sources/meta-ti/recipes-kernel/linux/linux-ti-staging_4.19.bb:do_assemble_fitimage) failed with exit code '1'
ERROR: u-boot-ti-staging-2019.01+gitAUTOINC+333c3e72d3-r32.tisdk6 do_package: Function failed: populate_srcipk_package (log file is located at /home/user/bwt/tisdk/build/arago-tmp-external-arm-toolchain/work/am57xx_hs_evm-linux-gnueabi/u-boot-ti-staging/2019.01+gitAUTOINC+333c3e72d3-r32.tisdk6/temp/log.do_package.16460)
ERROR: Logfile of failure stored in: /home/user/bwt/tisdk/build/arago-tmp-external-arm-toolchain/work/am57xx_hs_evm-linux-gnueabi/u-boot-ti-staging/2019.01+gitAUTOINC+333c3e72d3-r32.tisdk6/temp/log.do_package.16460
Log data follows:
| DEBUG: Executing python function sstate_task_prefunc
| DEBUG: Python function sstate_task_prefunc finished
| DEBUG: Executing python function extend_recipe_sysroot
| NOTE: Direct dependencies are ['virtual:native:/home/user/bwt/tisdk/sources/oe-core/meta/recipes-devtools/flex/flex_2.6.0.bb:do_populate_sysroot', '/home/user/bwt/tisdk/sources/oe-core/meta/recipes-devtools/quilt/quilt-native_0.65.bb:do_populate_sysroot', 'virtual:native:/home/user/bwt/tisdk/sources/oe-core/meta/recipes-devtools/pseudo/pseudo_git.bb:do_populate_sysroot', '/home/user/bwt/tisdk/sources/oe-core/meta/recipes-devtools/python/python-native_2.7.16.bb:do_populate_sysroot', '/home/user/bwt/tisdk/sources/meta-linaro/meta-linaro-toolchain/recipes-devtools/external-arm-toolchain/external-arm-toolchain.bb:do_populate_sysroot', 'virtual:native:/home/user/bwt/tisdk/sources/oe-core/meta/recipes-kernel/dtc/dtc_1.4.7.bb:do_populate_sysroot', 'virtual:native:/home/user/bwt/tisdk/sources/oe-core/meta/recipes-devtools/dwarfsrcfiles/dwarfsrcfiles.bb:do_populate_sysroot', 'virtual:native:/home/user/bwt/tisdk/sources/oe-core/meta/recipes-connectivity/openssl/openssl_1.1.1b.bb:do_populate_sysroot', 'virtual:native:/home/user/bwt/tisdk/sources/oe-core/meta/recipes-devtools/rpm/rpm_4.14.2.bb:do_populate_sysroot', 'virtual:native:/home/user/bwt/tisdk/sources/oe-core/meta/recipes-support/lzop/lzop_1.03.bb:do_populate_sysroot', 'virtual:native:/home/user/bwt/tisdk/sources/oe-core/meta/recipes-extended/bc/bc_1.07.1.bb:do_populate_sysroot', 'virtual:native:/home/user/bwt/tisdk/sources/oe-core/meta/recipes-extended/xz/xz_5.2.4.bb:do_populate_sysroot', 'virtual:native:/home/user/bwt/tisdk/sources/oe-core/meta/recipes-devtools/swig/swig_3.0.12.bb:do_populate_sysroot', 'virtual:native:/home/user/bwt/tisdk/sources/oe-core/meta/recipes-devtools/bison/bison_3.0.4.bb:do_populate_sysroot']
| NOTE: Installed into sysroot: []
| NOTE: Skipping as already exists in sysroot: ['flex-native', 'quilt-native', 'pseudo-native', 'python-native', 'external-arm-toolchain', 'dtc-native', 'dwarfsrcfiles-native', 'openssl-native', 'rpm-native', 'lzop-native', 'bc-native', 'xz-native', 'swig-native', 'bison-native', 'pkgconfig-native', 'autoconf-native', 'readline-native', 'expat-native', 'sqlite3-native', 'zlib-native', 'libtool-native', 'bzip2-native', 'gdbm-native', 'gnu-config-native', 'automake-native', 'db-native', 'gettext-minimal-native', 'popt-native', 'elfutils-native', 'python3-native', 'libarchive-native', 'file-native', 'nss-native', 'dbus-native', 'lzo-native', 'texinfo-dummy-native', 'libpcre-native', 'm4-native', 'ncurses-native', 'e2fsprogs-native', 'nspr-native', 'attr-native', 'util-linux-native']
| DEBUG: Python function extend_recipe_sysroot finished
| DEBUG: Executing python function do_package
| DEBUG: Executing python function package_get_auto_pr
| DEBUG: Python function package_get_auto_pr finished
| DEBUG: Executing python function perform_packagecopy
| DEBUG: Python function perform_packagecopy finished
| DEBUG: Executing python function split_and_strip_files
| DEBUG: Python function split_and_strip_files finished
| DEBUG: Executing python function fixup_perms
| DEBUG: Python function fixup_perms finished
| DEBUG: Executing python function package_do_split_locales
| DEBUG: No locale files in this package
| DEBUG: Python function package_do_split_locales finished
| DEBUG: Executing python function populate_packages
| DEBUG: Python function populate_packages finished
| DEBUG: Executing shell function populate_srcipk_package
| cp: cannot stat '/home/user/bwt/tisdk/build/arago-tmp-external-arm-toolchain/work/am57xx_hs_evm-linux-gnueabi/u-boot-ti-staging/2019.01+gitAUTOINC+333c3e72d3-r32.tisdk6/srcipk-staging/board-support/u-boot-2019.01+gitAUTOINC+333c3e72d3-g/.': No such file or directory
| WARNING: /home/user/bwt/tisdk/build/arago-tmp-external-arm-toolchain/work/am57xx_hs_evm-linux-gnueabi/u-boot-ti-staging/2019.01+gitAUTOINC+333c3e72d3-r32.tisdk6/temp/run.populate_srcipk_package.16460:1 exit 1 from 'cp -Prf --preserve=mode,timestamps --no-preserve=ownership /home/user/bwt/tisdk/build/arago-tmp-external-arm-toolchain/work/am57xx_hs_evm-linux-gnueabi/u-boot-ti-staging/2019.01+gitAUTOINC+333c3e72d3-r32.tisdk6/srcipk-staging/board-support/u-boot-2019.01+gitAUTOINC+333c3e72d3-g/. /home/user/bwt/tisdk/build/arago-tmp-external-arm-toolchain/work/am57xx_hs_evm-linux-gnueabi/u-boot-ti-staging/2019.01+gitAUTOINC+333c3e72d3-r32.tisdk6/packages-split/u-boot-ti-staging-src/board-support/u-boot-2019.01+gitAUTOINC+333c3e72d3-g'
| DEBUG: Python function do_package finished
| ERROR: Function failed: populate_srcipk_package (log file is located at /home/user/bwt/tisdk/build/arago-tmp-external-arm-toolchain/work/am57xx_hs_evm-linux-gnueabi/u-boot-ti-staging/2019.01+gitAUTOINC+333c3e72d3-r32.tisdk6/temp/log.do_package.16460)
ERROR: Task (/home/user/bwt/tisdk/sources/meta-ti/recipes-bsp/u-boot/u-boot-ti-staging_2019.01.bb:do_package) failed with exit code '1'
NOTE: Tasks Summary: Attempted 1313 tasks of which 1309 didn't need to be rerun and 2 failed.
Summary: 2 tasks failed:
/home/user/bwt/tisdk/sources/meta-ti/recipes-kernel/linux/linux-ti-staging_4.19.bb:do_assemble_fitimage
/home/user/bwt/tisdk/sources/meta-ti/recipes-bsp/u-boot/u-boot-ti-staging_2019.01.bb:do_package
Summary: There were 3 WARNING messages shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.