HI, Dear.
I'm using TMS320C5515 MDK for ECG with CCS v4.
However, when i do the quick start installaion guide, after the step "build active project" with led example,
to load program I do right click on "led.out" but I can't find "Load Program" on CCS v4.0
What I have to do to correctly load program.
after this situaion, I debug LED project and just in the step for UART the project is stopped.
So, I run (actually debug mode