Hi Champs:
The customer uses the TDA4 for being their PCB.
May you help to check this issue log?
How to solve it?
BR Rio
U-Boot SPL 2021.01 (Apr 13 2022 - 11:00:34 +0800)
Model: Texas Instruments K3 J721E SoC
Board: J721EX-PM2-SOM rev E8
SYSFW ABI: 3.1 (firmware rev 0x0016 '22.1.1--v2022.01 (Terrific Llam')
i2c_write: error waiting for data ACK (status=0x116)
read error from device: 41c8639c register: x!
i2c_write: error waiting for data ACK (status=0x116)
write error to device: 41c8639c register: x!
esm_pmic esm: clearing ESM irqs failed: -5
ESM PMIC init failed: -5
i2c_write: error waiting for data ACK (status=0x116)
write error to device: 41c8639c register: x!
esm_pmic esm: clearing ESM irqs failed: -5
ESM PMIC init failed: -5
Trying to boot from MMC2
Starting ATF on ARM64 core...
NOTICE: BL31: v2.5(release):08.01.00.006-dirty
NOTICE: BL31: Built : 21:03:57, Mar 23 2022
U-Boot SPL 2021.01 (Apr 13 2022 - 11:00:28 +0800)
Model: Texas Instruments K3 J721E SoC
Board: J721EX-PM2-SOM rev E8
SYSFW ABI: 3.1 (firmware rev 0x0016 '22.1.1--v2022.01 (Terrific Llam')
Detected: J7X-BASE-CPB rev E3
Detected: J7X-VSC8514-ETH rev E2
Trying to boot from MMC2
U-Boot 2021.01 (Apr 13 2022 - 11:00:28 +0800)
SoC: J721E SR1.1
Model: Texas Instruments K3 J721E SoC
Board: J721EX-PM2-SOM rev E8
DRAM: 4 GiB
Flash: 0 Bytes
MMC: sdhci@4f80000: 0, sdhci@4fb0000: 1
In: serial@2800000
Out: serial@2800000
Err: serial@2800000
am65_cpsw_nuss ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA00101 cpsw_ver: 0x6BA80100 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000
Detected: J7X-BASE-CPB rev E3
Detected: J7X-VSC8514-ETH rev E2
cdns,sierra serdes@5000000: PHY not found 0x7364 vs 0x0
Sierra init failed:-22
"Synchronous Abort" handler, esr 0x96000005
elr: 000000008082a878 lr : 000000008080350c (reloc)
elr: 00000000fff0e878 lr : 00000000ffee750c
x0 : 0000000000000003 x1 : 00000003ffffff80
x2 : 0000000000000070 x3 : 0000000400000000
x4 : 0000000002800000 x5 : 00000000fdeae2b8
x6 : 0000000000000032 x7 : 0000000000000001
x8 : 0000000000000001 x9 : 0000000000000008
x10: 00000000ffffffd0 x11: 000000000000000d
x12: 0000000000000006 x13: 000000000001869f
x14: 00000000fdeaea50 x15: 0000000000000002
x16: 00000000fff4ccfc x17: 0000000000000000
x18: 00000000fdec3df0 x19: 0000000000000000
x20: 0000000000000000 x21: 00000000fffa5988
x22: 00000000fffa7384 x23: 00000000800b76ae
x24: 00000000fffa7000 x25: 00000000deadbeef
x26: 0000000000000005 x27: 0000000000000000
x28: 0000000000000000 x29: 00000000fdeae960
Code: aa0003e2 52800000 f8470c41 d1020021 (f8480c23)
Resetting CPU ...
resetting ...