This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6442: Enabling fTPM

Part Number: AM6442

Hello,

I am trying to enable fTPM device driver (char/tpm_ftpm_tee) on the AM6442 SK board. I have enabled OPTEE, TPM and fTPM support in Kernel config. When I boot using the new kernel, the /dev/tee0 and /dev/teepriv0 devices are created, but no /dev/tpm0. I would like to know if there are additional steps required to do the same.

Thanks and Regards

  • Hi,

    I looked up the kernel source code in Processor SDK for AM64x, the ftpm driver is not TI platform dependent, the driver seems depending on kernel config TCG_FTPM_TEE and device tree bindings with compatible "microsoft,ftpm". However I don't find the DT binding document for "microsoft,ftpm" in kernel, and there is no any reference in kernel using this driver. Since ftpm is not a TI driver, we won't be able to provide any further details on enabling it. Recommend you asking the Linux community for support.