This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

compile qnx:TI RTOS 08_00 version without ti-optee-os folder

I try to download form ti-optee-os.git by "git clone git://git.ti.com/optee/ti-optee-os.git"

but there are some branch 

  remotes/origin/HEAD -> origin/master
  remotes/origin/master
  remotes/origin/ti-optee-os
  remotes/origin/ti-optee-os-next
  remotes/origin/ti_optee_os
  remotes/origin/ti_optee_os-next

Processor SDK QNX J721E 08_02_00 ?
Processor SDK QNX J721E 08_00_00 ?
  • Hi,

    For the PSDK RTOS releases, the optee is installed as part of running the ti-processor-sdk-rtos-j721e-evm-08_00_00_12/psdk_rtos/scripts/setup_psdk_rtos.sh.

    The setup_psdk_rtos.sh, script can be referenced to see the git commands being used for cloning.  Recommendation is to follow the same commands being used from the setup_psdk_rtos.sh, to ensure alignment with the SDK that is in use.

    Regards,

    kb