This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: TDA4 Jacinto 7 board troubleshooting

Part Number: TDA4VM

Hi Experts,

Our customer is having hardware trouble with TDA4 board they are using.

They applied DC 12V-10A power to the board and the Red light blinks once on LD3 and booting does not work. there is also no yellow light on LD5,6,7 but I confirmed that the LD2 continues to light on yellow. The board also has no physical damage.

They have been using the board continuously and are applying a Tc temperature of 125'C to the memory for the memory test. and the issue has occurred that the power does not turn on suddenly.

Does this mean that the board is dead? is there any other reason behind this?

Thanks for the help.

Regards,

Marvin