(I am posting here so that this thread is not auto closed. We are still interested.)
On Linux-RT SDK 8.2:
'ethtool -s eth1 speed 1000 duplex full autoneg on' does not work for when eth1 and eth5 is connected by cable.
Console log is attached as "minicom-loop-not-up-afterMAU-change.log".
U-Boot SPL 2021.01-g44a87e3ab8 (Mar 24 2022 - 06:00:43 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0016 '22.1.1--v2022.01 (Terrific Llam')
SPL initial stack usage: 1416 bytes
Trying to boot from MMC2
spl_load_fit_image: Skip load 'dm': image size is 0!
Starting ATF on ARM64 core...
NOTICE: BL31: v2.5(release):08.01.00.006-dirty
NOTICE: BL31: Built : 05:29:41, Mar 24 2022
U-Boot SPL 2021.01-g44a87e3ab8 (Mar 24 2022 - 05:30:44 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0016 '22.1.1--v2022.01 (Terrific Llam')
Detected: Silicon SR2.0
i2c_omap i2c@42120000: pinctrl_select_state_full: uclass_get_device_by_phandle_id: err=-19
Detected: AM6-IDKAPPEVM rev A
Detected: SER-PCIE2LEVM rev A
Trying to boot from MMC2
U-Boot 2021.01-g44a87e3ab8 (Mar 24 2022 - 05:30:44 +0000)
SoC: AM65X SR2.0
Model: Texas Instruments AM654 Base Board
Board: AM6-COMPROCEVM rev A
DRAM: 4 GiB
MMC: sdhci@4f80000: 0, sdhci@4fa0000: 1
Loading Environment from MMC... OK
In: serial
Out: serial
Err: serial
am65_cpsw_nuss ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA00102 cpsw_ver: 0x6BA80102 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000
Detected: Silicon SR2.0
Detected: AM6-IDKAPPEVM rev A
Detected: SER-PCIE2LEVM rev A
Net: eth1: icssg2-eth, eth0: ethernet@46000000port@1
Hit any key to stop autoboot: 2 1 0
switch to partitions #0, OK
mmc1 is current device
SD/MMC found on device 1
Failed to load 'boot.scr'
1011 bytes read in 4 ms (246.1 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc1 ...
Running uenvcmd ...
Using board_name = am65x
18231808 bytes read in 758 ms (22.9 MiB/s)
64207 bytes read in 7 ms (8.7 MiB/s)
11268 bytes read in 5 ms (2.1 MiB/s)
2333 bytes read in 5 ms (455.1 KiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 000000008feed000, end 000000008fffffff ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000] Linux version 5.10.100-rt62-g204ec708dc (oe-user@oe-host) (aarch64-none-linux-gnu-gcc (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 9.2.1 20191025, GNU ld (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 2.33.1.20191209) #1 SMP PREEMPT_RT Thu Mar 24 05:32:52 UTC 2022
[ 0.000000] Machine model: Texas Instruments AM654 Base Board
[ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
[ 0.000000] printk: bootconsole [ns16550a0] enabled
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node r5f-memory@a1100000, compatible id shared-dma-pool
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal [mem 0x0000000100000000-0x00000008ffffffff]
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x000000009e7fffff]
[ 0.000000] node 0: [mem 0x000000009e800000-0x00000000a20fffff]
[ 0.000000] node 0: [mem 0x00000000a2100000-0x00000000ffffffff]
[ 0.000000] node 0: [mem 0x0000000880000000-0x00000008ffffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000008ffffffff]
[ 0.000000] On node 0 totalpages: 1048576
[ 0.000000] DMA zone: 8192 pages used for memmap
[ 0.000000] DMA zone: 0 pages reserved
[ 0.000000] DMA zone: 524288 pages, LIFO batch:63
[ 0.000000] Normal zone: 8192 pages used for memmap
[ 0.000000] Normal zone: 524288 pages, LIFO batch:63
[ 0.000000] cma: Reserved 24 MiB at 0x00000000fe800000
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.2
[ 0.000000] percpu: Embedded 18 pages/cpu s34752 r8192 d30784 u73728
[ 0.000000] pcpu-alloc: s34752 r8192 d30784 u73728 alloc=18*4096
[ 0.000000] pcpu-alloc: [0] 0 [0] 1 [0] 2 [0] 3
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: ARM erratum 845719
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1032192
[ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),128k(ospi.env),128k(ospi.env.backup),1m(ospi.sysfw),57216k@8m(ospi.rootfs),128k(ospi.phypattern) root=PARTUUID=f40e08ce-02 rw rootfstype=ext4 rootwait
[ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] software IO TLB: mapped [mem 0x00000000fa800000-0x00000000fe800000] (64MB)
[ 0.000000] Memory: 3946716K/4194304K available (10624K kernel code, 1164K rwdata, 4148K rodata, 1728K init, 438K bss, 223012K reserved, 24576K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
[ 0.000000] rcu: RCU priority boosting: priority 1 delay 500 ms.
[ 0.000000] rcu: RCU_SOFTIRQ processing moved to rcuc kthreads.
[ 0.000000] No expedited grace period (rcu_normal_after_boot).
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 960 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] GICv3: Distributor has no Range Selector support
[ 0.000000] GICv3: 16 PPIs implemented
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000
[ 0.000000] ITS [mem 0x01820000-0x0182ffff]
[ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[ 0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[ 0.000000] ITS@0x0000000001820000: allocated 524288 Devices @880800000 (flat, esz 8, psz 64K, shr 0)
[ 0.000000] ITS: using cache flushing for cmd queue
[ 0.000000] GICv3: using LPI property table @0x0000000880040000
[ 0.000000] GIC: using cache flushing for LPI property table
[ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000880050000
[ 0.000000] random: get_random_bytes called from start_kernel+0x320/0x4c8 with crng_init=0
[ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[ 0.000000] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[ 0.008696] Console: colour dummy device 80x25
[ 0.013313] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[ 0.024035] pid_max: default: 32768 minimum: 301
[ 0.028900] LSM: Security Framework initializing
[ 0.033719] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.041335] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.051554] rcu: Hierarchical SRCU implementation.
[ 0.057162] Platform MSI: msi-controller@1820000 domain created
[ 0.063586] PCI/MSI: /bus@100000/interrupt-controller@1800000/msi-controller@1820000 domain created
[ 0.073041] EFI services will not be available.
[ 0.078040] smp: Bringing up secondary CPUs ...
[ 0.084009] Detected VIPT I-cache on CPU1
[ 0.088158] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000
[ 0.095221] GICv3: CPU1: using allocated LPI pending table @0x0000000880060000
[ 0.102683] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.110958] Detected VIPT I-cache on CPU2
[ 0.115125] GICv3: CPU2: found redistributor 100 region 0:0x00000000018c0000
[ 0.122368] GICv3: CPU2: using allocated LPI pending table @0x0000000880070000
[ 0.129839] CPU2: Booted secondary processor 0x0000000100 [0x410fd034]
[ 0.138015] Detected VIPT I-cache on CPU3
[ 0.142158] GICv3: CPU3: found redistributor 101 region 0:0x00000000018e0000
[ 0.149398] GICv3: CPU3: using allocated LPI pending table @0x0000000880080000
[ 0.156845] CPU3: Booted secondary processor 0x0000000101 [0x410fd034]
[ 0.163728] smp: Brought up 1 node, 4 CPUs
[ 0.167970] SMP: Total of 4 processors activated.
[ 0.172819] CPU features: detected: 32-bit EL0 Support
[ 0.178111] CPU features: detected: CRC32 instructions
[ 0.198438] CPU: All CPU(s) started at EL2
[ 0.202684] alternatives: patching kernel code
[ 0.208758] devtmpfs: initialized
[ 0.225915] KASLR disabled due to lack of seed
[ 0.230792] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.240814] futex hash table entries: 1024 (order: 5, 131072 bytes, linear)
[ 0.249298] pinctrl core: initialized pinctrl subsystem
[ 0.255345] DMI not present or invalid.
[ 0.259925] NET: Registered protocol family 16
[ 0.266812] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations
[ 0.274293] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.282644] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.291600] thermal_sys: Registered thermal governor 'step_wise'
[ 0.292389] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.305651] ASID allocator initialised with 65536 entries
[ 0.362745] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.369708] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.376610] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.383542] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.392091] cryptd: max_cpu_qlen set to 1000
[ 0.401727] k3-chipinfo 43000014.chipid: Family:AM65X rev:SR2.0 JTAGID[0x1bb5a02f] Detected
[ 0.411170] vcc3v3_io: supplied by evm_12v0
[ 0.417019] iommu: Default domain type: Translated
[ 0.422998] SCSI subsystem initialized
[ 0.427702] mc: Linux media interface: v0.10
[ 0.432147] videodev: Linux video capture interface: v2.00
[ 0.437922] pps_core: LinuxPPS API ver. 1 registered
[ 0.443061] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.452453] PTP clock support registered
[ 0.456518] EDAC MC: Ver: 3.0.0
[ 0.461272] FPGA manager framework
[ 0.464917] Advanced Linux Sound Architecture Driver Initialized.
[ 0.472423] clocksource: Switched to clocksource arch_sys_counter
[ 0.478943] VFS: Disk quotas dquot_6.6.0
[ 0.483049] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.499160] NET: Registered protocol family 2
[ 0.504040] IP idents hash table entries: 65536 (order: 7, 524288 bytes, linear)
[ 0.514359] tcp_listen_portaddr_hash hash table entries: 2048 (order: 5, 131072 bytes, linear)
[ 0.523455] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.532021] TCP bind hash table entries: 32768 (order: 8, 1835008 bytes, linear)
[ 0.542033] TCP: Hash tables configured (established 32768 bind 32768)
[ 0.549070] UDP hash table entries: 2048 (order: 6, 262144 bytes, linear)
[ 0.556538] UDP-Lite hash table entries: 2048 (order: 6, 262144 bytes, linear)
[ 0.564560] NET: Registered protocol family 1
[ 0.569986] RPC: Registered named UNIX socket transport module.
[ 0.576194] RPC: Registered udp transport module.
[ 0.581032] RPC: Registered tcp transport module.
[ 0.585862] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.592486] PCI: CLS 0 bytes, default 64
[ 0.597765] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
[ 0.612712] Initialise system trusted keyrings
[ 0.617599] workingset: timestamp_bits=46 max_order=20 bucket_order=0
[ 0.631283] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.638226] NFS: Registering the id_resolver key type
[ 0.643504] Key type id_resolver registered
[ 0.647832] Key type id_legacy registered
[ 0.652083] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.658989] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.666927] 9p: Installing v9fs 9p2000 file system support
[ 0.724962] Key type asymmetric registered
[ 0.729213] Asymmetric key parser 'x509' registered
[ 0.734290] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[ 0.741958] io scheduler mq-deadline registered
[ 0.746613] io scheduler kyber registered
[ 0.754188] pinctrl-single 4301c000.pinctrl: 70 pins, size 280
[ 0.760992] pinctrl-single 11c000.pinctrl: 185 pins, size 740
[ 0.767120] pinctrl-single 11c2e8.pinctrl: 9 pins, size 36
[ 0.780902] k3-ringacc 2b800000.ringacc: Failed to get MSI domain
[ 0.787337] k3-ringacc 3c000000.ringacc: Failed to get MSI domain
[ 0.799113] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 0.828152] brd: module loaded
[ 0.843264] loop: module loaded
[ 0.847602] megasas: 07.714.04.00-rc1
[ 0.857881] tun: Universal TUN/TAP device driver, 1.6
[ 0.864058] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[ 0.870534] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 0.876765] sky2: driver version 1.30
[ 0.882141] VFIO - User Level meta-driver version: 0.3
[ 0.889038] i2c /dev entries driver
[ 0.894501] sdhci: Secure Digital Host Controller Interface driver
[ 0.900886] sdhci: Copyright(c) Pierre Ossman
[ 0.906007] sdhci-pltfm: SDHCI platform and OF driver helper
[ 0.913720] ti-sci bus@100000:bus@28380000:bus@42040000:dmsc: invalid resource
[ 0.921402] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 0.929812] optee: probing for conduit method.
[ 0.934420] optee: revision 3.12 (3d47a131)
[ 0.935103] optee: initialized driver
[ 0.946298] NET: Registered protocol family 17
[ 0.951149] 9pnet: Installing 9P2000 support
[ 0.955632] Key type dns_resolver registered
[ 0.960481] printk: bootconsole [ns16550a0]: printing thread started
[ 0.960539] Loading compiled-in X.509 certificates
[ 0.973940] k3-ringacc 2b800000.ringacc: Failed to get MSI domain
[ 0.974268] k3-ringacc 3c000000.ringacc: Failed to get MSI domain
[ 0.982293] ti-sci bus@100000:bus@28380000:bus@42040000:dmsc: invalid resource
[ 0.982752] ti-sci bus@100000:bus@28380000:bus@42040000:dmsc: ABI: 3.1 (firmware rev 0x0016 '22.1.1--v2022.01 (Terrific Llam')
[ 1.057069] random: fast init done
[ 1.078701] omap_i2c 42120000.i2c: bus 0 rev0.12 at 400 kHz
[ 1.080151] omap_i2c 40b00000.i2c: bus 1 rev0.12 at 100 kHz
[ 1.082574] pca953x 2-0021: supply vcc not found, using dummy regulator
[ 1.082783] pca953x 2-0021: using no AI
[ 1.105307] omap_i2c 2000000.i2c: bus 2 rev0.12 at 400 kHz
[ 1.106568] omap_i2c 2010000.i2c: bus 3 rev0.12 at 400 kHz
[ 1.107729] omap_i2c 2020000.i2c: bus 4 rev0.12 at 400 kHz
[ 1.108902] omap_i2c 2030000.i2c: bus 5 rev0.12 at 100 kHz
[ 1.110350] ti-sci-intr bus@100000:bus@28380000:bus@42040000:interrupt-controller2: Interrupt Router 156 domain created
[ 1.110627] ti-sci-intr bus@100000:interrupt-controller0: Interrupt Router 100 domain created
[ 1.110885] ti-sci-intr bus@100000:main-navss:interrupt-controller1: Interrupt Router 182 domain created
[ 1.111343] ti-sci-inta 33d00000.interrupt-controller: Interrupt Aggregator domain 179 created
[ 1.126688] keystone-pcie 5500000.pcie: host bridge /bus@100000/pcie@5500000 ranges:
[ 1.126727] OF: /bus@100000/pcie@5500000: Missing device_type
[ 1.126764] keystone-pcie 5500000.pcie: IO 0x0010020000..0x001002ffff -> 0x0000000000
[ 1.126793] keystone-pcie 5500000.pcie: MEM 0x0010030000..0x0017ffffff -> 0x0010030000
[ 2.127560] keystone-pcie 5500000.pcie: Phy link never came up
[ 2.127767] keystone-pcie 5500000.pcie: PCI host bridge to bus 0000:00
[ 2.127781] pci_bus 0000:00: root bus resource [bus 00-ff]
[ H��2.127793] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
[ 2.127802] pci_bus 0000:00: root bus resource [mem 0x10030000-0x17ffffff]
[ 2.153702] printk: console [ttyS2]: printing thread started
[ 2.127881] pci 0000:00:00.0: [104c:b00c] type 01 class 0x060400
[ 2.153729] printk: console [ttyS2] enabled
[ 2.153736] printk: bootconsole [ns16550a0] disabled
[ 2.172768] printk: bootconsole [ns16550a0]: printing thread stopped
[ 2.174126] 2810000.serial: ttyS3 at MMIO 0x2810000 (irq = 30, base_baud = 3000000) is a 8250
[ 2.175209] 2820000.serial: ttyS4 at MMIO 0x2820000 (irq = 31, base_baud = 3000000) is a 8250
[ 2.232463] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 2.235028] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867
[ 2.235162] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00102, cpsw version 0x6BA80102 Ports: 2 quirks:00000000
[ 2.238414] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010b, freq:200000000, add_val:4 pps:0
[ 2.242558] mmc0: CQHCI version 5.10
[ 2.257409] pca953x 0-0039: supply vcc not found, using dummy regulator
[ 2.257669] pca953x 0-0039: using no AI
[ 2.282389] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fc7100
[ 2.282994] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fc7100
[ 2.284706] mmc0: SDHCI controller on 4f80000.mmc [4f80000.mmc] using ADMA 64-bit
[ 2.286739] ti-udma 285c0000.dma-controller: Channels: 28 (tchan: 14, rchan: 14, gp-rflow: 16)
[ 2.294407] ti-udma 31150000.dma-controller: Channels: 119 (tchan: 53, rchan: 66, gp-rflow: 64)
[ 2.308864] spi-nor spi7.0: mt35xu512aba (65536 Kbytes)
[ 2.308910] 8 cmdlinepart partitions found on MTD device 47040000.spi.0
[ 2.308918] Creating 8 MTD partitions on "47040000.spi.0":
[ 2.308925] 0x000000000000-0x000000080000 : "ospi.tiboot3"
[ 2.310752] 0x000000080000-0x000000280000 : "ospi.tispl"
[ 2.312305] 0x000000280000-0x000000680000 : "ospi.u-boot"
[ 2.313902] 0x000000680000-0x0000006a0000 : "ospi.env"
[ 2.315457] 0x0000006a0000-0x0000006c0000 : "ospi.env.backup"
[ 2.317046] 0x0000006c0000-0x0000007c0000 : "ospi.sysfw"
[ 2.318617] 0x000000800000-0x000003fe0000 : "ospi.rootfs"
[ 2.320197] 0x000003fe0000-0x000004000000 : "ospi.phypattern"
[ 2.333470] spi-nor spi9.0: n25q128a13 (16384 Kbytes)
[ 2.371983] mmc0: Command Queue Engine enabled
[ 2.372009] mmc0: new HS200 MMC card at address 0001
[ 2.372824] mmcblk0: mmc0:0001 S0J56X 14.8 GiB
[ 2.373080] mmcblk0boot0: mmc0:0001 S0J56X partition 1 31.5 MiB
[ 2.373341] mmcblk0boot1: mmc0:0001 S0J56X partition 2 31.5 MiB
[ 2.373638] mmcblk0rpmb: mmc0:0001 S0J56X partition 3 4.00 MiB, chardev (237:0)
[ 2.376510] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 2.379520] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867
[ 2.379676] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00102, cpsw version 0x6BA80102 Ports: 2 quirks:00000000
[ 2.381378] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48
[ 2.382315] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
[ 2.382325] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
[ 2.383435] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:200000000, add_val:4 pps:0
[ 2.387618] vdd_mmc1_sd: supplied by vcc3v3_io
[ 2.389845] debugfs: Directory 'pd:121' with parent 'pm_genpd' already present!
[ 2.389920] debugfs: Directory 'pd:120' with parent 'pm_genpd' already present!
[ 2.390262] mmc1: CQHCI version 5.10
[ 2.393570] input: gpio-keys as /devices/platform/gpio-keys/input/input0
[ 2.416591] ALSA device list:
[ 2.416602] No soundcards found.
[ 3.314314] mmc1: SDHCI controller on 4fa0000.mmc [4fa0000.mmc] using ADMA 64-bit
[ 3.314930] Waiting for root device PARTUUID=f40e08ce-02...
[ 3.372453] mmc1: new ultra high speed SDR104 SDHC card at address aaaa
[ 3.373304] mmcblk1: mmc1:aaaa SA08G 7.40 GiB
[ 3.375280] mmcblk1: p1 p2
[ 3.706743] EXT4-fs (mmcblk1p2): recovery complete
[ 3.707630] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)
[ 3.707726] VFS: Mounted root (ext4 filesystem) on device 179:98.
[ 3.708715] devtmpfs: mounted
[ 3.710123] Freeing unused kernel memory: 1728K
[ 3.710299] Run /sbin/init as init process
[ 3.836877] systemd[1]: System time before build time, advancing clock.
[ 3.886874] NET: Registered protocol family 10
[ 3.888537] Segment Routing with IPv6
[ 3.908090] systemd[1]: systemd 244.5+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
[ 3.908905] systemd[1]: Detected architecture arm64.
Welcome to Arago 2021.09!
[ 3.966180] systemd[1]: Set hostname to <am65xx-evm>.
[ 4.349673] systemd[1]: /lib/systemd/system/docker.socket:6: ListenStream= references a path below legacy directory /var/run/, updating /var/run/docker.sock → /run/docker.sock; please update the unit file accordingly.
[ 4.485051] random: systemd: uninitialized urandom read (16 bytes read)
[ 4.485472] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.
[ 4.485533] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)
[ 4.491091] systemd[1]: Created slice system-getty.slice.
[ OK ] Created slice system-getty.slice.
[ OK ] Created slice system-serial\x2dgett[ 4.536687] random: systemd: uninitialized urandom read (16 bytes read)
[ 4.539066] systemd[1]: Created slice system-serial\x2dgetty.slice.
y.slice.
[ OK ] Created slice User and Session Slic[ 4.568642] random: systemd: uninitialized urandom read (16 bytes read)
e.
[ 4.570639] systemd[1]: Created slice User and Session Slice.
[ OK ] Started Dispatch Password …ts to [ 4.590123] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
Console Directory Watch.
[ OK ] Started Forward Password R…uests [ 4.612854] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
to Wall Directory Watch.
[ OK ] Reached target Paths.[ 4.636806] systemd[1]: Reached target Paths.
[ OK ] Reached target Remote File Systems 4.656637] systemd[1]: Reached target Remote File Systems.
[0m.
[ OK ] Reached target Slices.[ 4.676593] systemd[1]: Reached target Slices.
[ OK ] Reached target Swap.
[ 4.696600] systemd[1]: Reached target Swap.
[ OK ] Listening on RPCbind Server Activat[ 4.711759] systemd[1]: Listening on RPCbind Server Activation Socket.
ion Socket.
[ OK ] Reached target RPC Port Mapper.[ 4.732711] systemd[1]: Reached target RPC Port Mapper.
[ OK ] Listening on Process Core Dump Sock[ 4.760068] systemd[1]: Listening on Process Core Dump Socket.
et.
[ OK ] Listening on initctl Compatibility [ 4.780989] systemd[1]: Listening on initctl Compatibility Named Pipe.
Named Pipe.
[ 4.815679] systemd[1]: Condition check resulted in Journal Audit Socket being skipped.
[ 4.816760] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket.[ 4.845349] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Network Service Netlin[ 4.865514] systemd[1]: Listening on Network Service Netlink Socket.
k Socket.
[ OK ] Listening on udev Control Socket 4.889223] systemd[1]: Listening on udev Control Socket.
m.
[ OK ] Listening on udev Kernel Socket[ 4.912995] systemd[1]: Listening on udev Kernel Socket.
.
Mounting Huge Pages File System...
[ 4.939515] systemd[1]: Mounting Huge Pages File System...
Mounting POSIX Message Queue File System..[ 4.957187] systemd[1]: Mounting POSIX Message Queue File System...
.
Mounting Kernel Debug File System...
[ 4.987186] systemd[1]: Mounting Kernel Debug File System...
Mounting Temporary Directory (/tmp)...[ 5.006184] systemd[1]: Mounting Temporary Directory (/tmp)...
Starting Create list of st…odes for the curr[ 5.035655] systemd[1]: Starting Create list of static device nodes for the current kernel...
ent kernel...
Starting Start psplash boot splash screen.[ 5.066758] systemd[1]: Starting Start psplash boot splash screen...
..
Starting RPC Bind...
[ 5.097090] systemd[1]: Starting RPC Bind...
[ 5.108988] systemd[1]: Condition check resulted in File System Check on Root Device being skipped.
[ 5.117462] systemd[1]: Starting Journal Service...
Starting Journal Service...
Starting Load Kernel Modules...
[ 5.150318] systemd[1]: Starting Load Kernel Modules...
Starting Remount Root and Kernel File Systems 5.167673] systemd[1]: Starting Remount Root and Kernel File Systems...
[0m...
[ 5.178550] cryptodev: loading out-of-tree module taints kernel.
[ 5.181418] cryptodev: driver 1.10 loaded.
[ 5.197408] EXT4-fs (mmcblk1p2): re-mounted. Opts: (null)
[ 5.201043] systemd[1]: Starting udev Coldplug all Devices...
Starting udev Coldplug all Devices...
[ OK ] Started RPC Bind.
[ 5.230834] systemd[1]: Started RPC Bind.
[ OK ] Mounted Huge Pages File System.[ 5.242095] systemd[1]: Mounted Huge Pages File System.
[ OK ] Mounted POSIX Message Queue File Sy[ 5.266129] systemd[1]: Mounted POSIX Message Queue File System.
stem.
[ OK ] Started Journal Service.
[ 5.289332] systemd[1]: Started Journal Service.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Mounted Temporary Directory (/tmp).
[ OK ] Started Create list of sta… nodes for the current kernel.
[FAILED] Failed to start Start psplash boot splash screen.
See 'systemctl status psplash-start.service' for details.
[DEPEND] Dependency failed for Star…progress communication helper.
[ OK ] Started Load Kernel Modules.
[ OK ] Started Remount Root and Kernel File Systems.
Mounting Kernel Configuration File System...
Starting Flush Journal to Persistent Storage...
[ 5.522896] systemd-journald[221]: Received client request to flush runtime journal.
Starting Apply Kernel Variables...
Starting Create Static Device Nodes in /dev...
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Create Static Device Nodes in /dev.
[ OK ] Reached target Local File Systems (Pre).
Mounting /media/ram...
Mounting /var/volatile...
Starting udev Kernel Device Manager...
[ OK ] Mounted /media/ram.
[ OK ] Mounted /var/volatile.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
[ OK ] Started Create Volatile Files and Directories.
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
[ OK ] Started udev Kernel Device Manager.
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ 8.309077] [drm] Initialized pvr 1.17.4948957 20110701 for 7000000.gpu on minor 0
[ 8.332572] random: crng init done
[ 8.332592] random: 7 urandom warning(s) missed due to ratelimiting
[ 8.532107] CAN device driver interface
[ 8.642151] cal 6f03000.cal: Neither port is configured, no point in staying up
[ 9.021433] platform 41000000.r5f: configured R5F for remoteproc mode
[ 9.022946] platform 41000000.r5f: assigned reserved memory node r5f-dma-memory@a0000000
[ 9.058535] remoteproc remoteproc0: 41000000.r5f is available
[ 9.067089] remoteproc remoteproc0: powering up 41000000.r5f
[ 9.067125] remoteproc remoteproc0: Booting fw image am65x-mcu-r5f0_0-fw, size 82412
[ 9.101415] remoteproc0#vdev0buffer: assigned reserved memory node r5f-dma-memory@a0000000
[ OK ] Started Load/Save Random Seed.
[ 9.206111] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 9.211606] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xd
[ 9.249247] remoteproc0#vdev0buffer: registered virtio0 (type 7)
[ 9.249278] remoteproc remoteproc0: remote processor 41000000.r5f is now up
[ 9.277630] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe
[ 9.365370] OF: graph: no port node found in /bus@100000/phy@4110000
[ 9.732542] davinci_mdio b032400.mdio: davinci mdio revision 1.7, bus freq 1000000
[ OK ] Started Network Time Synchronization.
[ 9.826952] davinci_mdio b032400.mdio: phy[0]: device b032400.mdio:00, driver TI DP83867
[ 9.826978] davinci_mdio b032400.mdio: phy[3]: device b032400.mdio:03, driver TI DP83867
[ OK ] Started udev Coldplug all Devices.
[ OK ] Reached target System Time Set.
[ OK ] Reached target System Time Synchronized.
Starting udev Wait for Complete Device Initialization...
[ 10.772542] davinci_mdio b132400.mdio: davinci mdio revision 1.7, bus freq 1000000
[ 11.015113] davinci_mdio b132400.mdio: phy[0]: device b132400.mdio:00, driver TI DP83867
[ 11.015138] davinci_mdio b132400.mdio: phy[3]: device b132400.mdio:03, driver TI DP83867
[ 11.054349] m_can_platform 40568000.mcan: m_can device registered (irq=25, version=32)
[ 11.186757] m_can_platform 40528000.mcan: m_can device registered (irq=23, version=32)
[ 11.260533] davinci_mdio b232400.mdio: davinci mdio revision 1.7, bus freq 1000000
[ 11.347304] davinci_mdio b232400.mdio: phy[0]: device b232400.mdio:00, driver TI DP83867
[ 11.347330] davinci_mdio b232400.mdio: phy[3]: device b232400.mdio:03, driver TI DP83867
[ 11.365950] remoteproc remoteproc1: b034000.pru is available
[ 11.366798] remoteproc remoteproc2: b004000.rtu is available
[ 11.367415] remoteproc remoteproc3: b00a000.txpru is available
[ 11.367941] remoteproc remoteproc4: b038000.pru is available
[ 11.372942] remoteproc remoteproc5: b006000.rtu is available
[ 11.373715] remoteproc remoteproc6: b00c000.txpru is available
[ 11.374292] remoteproc remoteproc7: b134000.pru is available
[ 11.375089] remoteproc remoteproc8: b104000.rtu is available
[ 11.375630] remoteproc remoteproc9: b10a000.txpru is available
[ 11.376029] remoteproc remoteproc10: b138000.pru is available
[ 11.377002] remoteproc remoteproc11: b106000.rtu is available
[ 11.377554] remoteproc remoteproc12: b10c000.txpru is available
[ 11.388708] remoteproc remoteproc13: b234000.pru is available
[ 11.389615] remoteproc remoteproc14: b204000.rtu is available
[ 11.390303] remoteproc remoteproc15: b20a000.txpru is available
[ 11.401251] remoteproc remoteproc16: b238000.pru is available
[ 11.402768] remoteproc remoteproc17: b206000.rtu is available
[ 11.407859] remoteproc remoteproc18: b20c000.txpru is available
[ 11.929159] omap_rng 4e10000.rng: Random Number Generator ver. 241b34c
[ OK ] Created slice system-systemd\x2dfsck.slice.
[ OK ] Found device /dev/mmcblk1p1.
Starting File System Check on /dev/mmcblk1p1 12.865794] usbcore: registered new interface driver usbfs
0m...
[ 12.880389] usbcore: registered new interface driver hub
[ 12.897748] usbcore: registered new device driver usb
[ OK ] Reached target Hardware activated USB gadget.
[ 13.212883] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller
[ 13.214825] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 1
[ 13.215000] xhci-hcd xhci-hcd.2.auto: hcc params 0x0298fe6d hci version 0x110 quirks 0x0000000000010010
[ 13.215380] xhci-hcd xhci-hcd.2.auto: irq 594, io mem 0x04010000
[ 13.216083] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10
[ 13.216101] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 13.216111] usb usb1: Product: xHCI Host Controller
[ 13.216118] usb usb1: Manufacturer: Linux 5.10.100-rt62-g204ec708dc xhci-hcd
[ 13.216125] usb usb1: SerialNumber: xhci-hcd.2.auto
[ 13.265430] icssg-prueth icssg0-eth: TI PRU ethernet driver initialized: dual EMAC mode
[ 13.438781] hub 1-0:1.0: USB hub found
[ 13.438867] hub 1-0:1.0: 1 port detected
[ 13.507703] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller
[ 13.507763] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 2
[ 13.507795] xhci-hcd xhci-hcd.2.auto: Host supports USB 3.0 SuperSpeed
[ 13.507909] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 13.508090] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 5.10
[ 13.508103] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 13.508113] usb usb2: Product: xHCI Host Controller
[ 13.508121] usb usb2: Manufacturer: Linux 5.10.100-rt62-g204ec708dc xhci-hcd
[ 13.508128] usb usb2: SerialNumber: xhci-hcd.2.auto
[ 13.591615] hub 2-0:1.0: USB hub found
[ 13.591712] hub 2-0:1.0: 1 port detected
[ 13.733635] icssg-prueth icssg2-eth: TI PRU ethernet driver initialized: dual EMAC mode
[ OK ] Started File System Check on /dev/mmcblk1p1.
[ 14.183606] icssg-prueth icssg1-eth: TI PRU ethernet driver initialized: dual EMAC mode
Mounting /run/media/mmcblk1p1...
[ OK ] Mounted /run/media/mmcblk1p1.
[ OK ] Started udev Wait for Complete Device Initialization.
[ OK ] Started Hardware RNG Entropy Gatherer Daemon.
[ OK ] Reached target System Initialization.
[ OK ] Started Daily rotation of log files.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Timers.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on D-Bus System Message Bus Socket.
Starting Docker Socket for the API.
[ OK ] Listening on dropbear.socket.
Starting Reboot and dump vmcore via kexec...
[ OK ] Listening on Docker Socket for the API.
[ OK ] Started Reboot and dump vmcore via kexec.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
[ OK ] Started Job spooling tools.
[ OK ] Started Periodic Command Scheduler.
[ OK ] Started D-Bus System Message Bus.
Starting Print notice about GPLv3 packages...
Starting IPv6 Packet Filtering Framework...
Starting IPv4 Packet Filtering Framework...
[ OK ] Started irqbalance daemon.
Starting Telephony service...
Starting rc.pvr.service...
Starting Login Service...
[ OK ] Started TEE Supplicant.
[ OK ] Started IPv6 Packet Filtering Framework.
[ OK ] Started IPv4 Packet Filtering Framework.
[ OK ] Reached target Network (Pre).
Starting Network Service...
[ OK ] Started Telephony service.
[ 15.053752] PVR_K: UM DDK-(4948957) and KM DDK-(4948957) match. [ OK ]
[ OK ] Listening on Load/Save RF …itch Status /dev/rfkill Watch.
[ OK ] Started rc.pvr.service.
[ 15.121674] Bluetooth: Core ver 2.22
[ 15.121876] NET: Registered protocol family 31
Starting weston.service...
[ 15.121883] Bluetooth: HCI device and connection manager initialized
[ 15.121910] Bluetooth: HCI socket layer initialized
[ 15.121925] Bluetooth: L2CAP socket layer initialized
[ 15.121954] Bluetooth: SCO socket layer initialized
[ OK ] Started weston.service.
Starting telnetd.service...
[ OK ] Started telnetd.service.
[ OK ] Started Network Service.
Starting Wait for Network to be Configured...
Starting Network Name Resolution...
[ 15.617134] remoteproc remoteproc10: powering up b138000.pru
[ 15.619909] remoteproc remoteproc10: Booting fw image ti-pruss/am65x-sr2-pru1-prueth-fw.elf, size 37540
[ 15.619952] remoteproc remoteproc10: unsupported resource 5
[ 15.619985] remoteproc remoteproc10: remote processor b138000.pru is now up
[ 15.620028] remoteproc remoteproc11: powering up b106000.rtu
[ 15.648626] remoteproc remoteproc11: Booting fw image ti-pruss/am65x-sr2-rtu1-prueth-fw.elf, size 30088
[ 15.648693] remoteproc remoteproc11: remote processor b106000.rtu is now up
[ 15.648741] remoteproc remoteproc12: powering up b10c000.txpru
[ 15.650161] remoteproc remoteproc12: Booting fw image ti-pruss/am65x-sr2-txpru1-prueth-fw.elf, size 35264
[ 15.650215] remoteproc remoteproc12: remote processor b10c000.txpru is now up
[ 15.672487] icssg-prueth icssg1-eth: settime timeout
[ 15.672912] pps pps0: new PPS source ptp2
[ 15.693715] TI DP83867 b132400.mdio:03: attached PHY driver [TI DP83867] (mii_bus:phy_addr=b132400.mdio:03, irq=POLL)
[ 15.693998] net eth6: started
[ 15.781669] remoteproc remoteproc7: powering up b134000.pru
[ 15.783772] remoteproc remoteproc7: Booting fw image ti-pruss/am65x-sr2-pru0-prueth-fw.elf, size 37264
[ 15.783810] remoteproc remoteproc7: unsupported resource 5
[ 15.783842] remoteproc remoteproc7: remote processor b134000.pru is now up
[ 15.783887] remoteproc remoteproc8: powering up b104000.rtu
[ 15.788566] remoteproc remoteproc8: Booting fw image ti-pruss/am65x-sr2-rtu0-prueth-fw.elf, size 30832
[ 15.788622] remoteproc remoteproc8: remote processor b104000.rtu is now up
[ 15.788668] remoteproc remoteproc9: powering up b10a000.txpru
[ 15.791867] remoteproc remoteproc9: Booting fw image ti-pruss/am65x-sr2-txpru0-prueth-fw.elf, size 36656
[ 15.791928] remoteproc remoteproc9: remote processor b10a000.txpru is now up
[ 15.816625] TI DP83867 b132400.mdio:00: attached PHY driver [TI DP83867] (mii_bus:phy_addr=b132400.mdio:00, irq=POLL)
[ 15.816915] net eth5: started
[ 15.885240] remoteproc remoteproc16: powering up b238000.pru
[ 15.885538] remoteproc remoteproc16: Booting fw image ti-pruss/am65x-sr2-pru1-prueth-fw.elf, size 37540
[ 15.885573] remoteproc remoteproc16: unsupported resource 5
[ 15.885605] remoteproc remoteproc16: remote processor b238000.pru is now up
[ 15.885644] remoteproc remoteproc17: powering up b206000.rtu
[ 15.885830] remoteproc remoteproc17: Booting fw image ti-pruss/am65x-sr2-rtu1-prueth-fw.elf, size 30088
[ 15.885871] remoteproc remoteproc17: remote processor b206000.rtu is now up
[ 15.885903] remoteproc remoteproc18: powering up b20c000.txpru
[ 15.886071] remoteproc remoteproc18: Booting fw image ti-pruss/am65x-sr2-txpru1-prueth-fw.elf, size 35264
[ 15.886115] remoteproc remoteproc18: remote processor b20c000.txpru is now up
[ 15.891492] icssg-prueth icssg2-eth: settime timeout
[ 15.892580] pps pps1: new PPS source ptp3
[ 15.912120] TI DP83867 b232400.mdio:03: attached PHY driver [TI DP83867] (mii_bus:phy_addr=b232400.mdio:03, irq=POLL)
[ 15.912483] net eth4: started
[ 15.973345] remoteproc remoteproc13: powering up b234000.pru
[ 15.973602] remoteproc remoteproc13: Booting fw image ti-pruss/am65x-sr2-pru0-prueth-fw.elf, size 37264
[ 15.973631] remoteproc remoteproc13: unsupported resource 5
[ 15.973662] remoteproc remoteproc13: remote processor b234000.pru is now up
[ 15.973699] remoteproc remoteproc14: powering up b204000.rtu
[ 15.973887] remoteproc remoteproc14: Booting fw image ti-pruss/am65x-sr2-rtu0-prueth-fw.elf, size 30832
[ OK ] Started Login Service.
[ 15.973924] remoteproc remoteproc14: remote processor b204000.rtu is now up
[ 15.973950] remoteproc remoteproc15: powering up b20a000.txpru
[ 15.974106] remoteproc remoteproc15: Booting fw image ti-pruss/am65x-sr2-txpru0-prueth-fw.elf, size 36656
[ 15.974150] remoteproc remoteproc15: remote processor b20a000.txpru is now up
[ 15.994375] TI DP83867 b232400.mdio:00: attached PHY driver [TI DP83867] (mii_bus:phy_addr=b232400.mdio:00, irq=POLL)
[ 15.994662] net eth3: started
[ 16.105125] remoteproc remoteproc4: powering up b038000.pru
[ 16.105434] remoteproc remoteproc4: Booting fw image ti-pruss/am65x-sr2-pru1-prueth-fw.elf, size 37540
[ 16.105466] remoteproc remoteproc4: unsupported resource 5
[ 16.105498] remoteproc remoteproc4: remote processor b038000.pru is now up
[ 16.105537] remoteproc remoteproc5: powering up b006000.rtu
[ 16.105706] remoteproc remoteproc5: Booting fw image ti-pruss/am65x-sr2-rtu1-prueth-fw.elf, size 30088
[ 16.105745] remoteproc remoteproc5: remote processor b006000.rtu is now up
[ 16.105772] remoteproc remoteproc6: powering up b00c000.txpru
[ 16.105918] remoteproc remoteproc6: Booting fw image ti-pruss/am65x-sr2-txpru1-prueth-fw.elf, size 35264
[ 16.105961] remoteproc remoteproc6: remote processor b00c000.txpru is now up
[ 16.111288] icssg-prueth icssg0-eth: settime timeout
[ 16.112569] pps pps2: new PPS source ptp4
[ 16.137540] TI DP83867 b032400.mdio:03: attached PHY driver [TI DP83867] (mii_bus:phy_addr=b032400.mdio:03, irq=POLL)
[ 16.137825] net eth2: started
[ 16.209180] remoteproc remoteproc1: powering up b034000.pru
[ 16.209425] remoteproc remoteproc1: Booting fw image ti-pruss/am65x-sr2-pru0-prueth-fw.elf, size 37264
[ 16.209458] remoteproc remoteproc1: unsupported resource 5
[ 16.209489] remoteproc remoteproc1: remote processor b034000.pru is now up
[ 16.209527] remoteproc remoteproc2: powering up b004000.rtu
[ 16.209668] remoteproc remoteproc2: Booting fw image ti-pruss/am65x-sr2-rtu0-prueth-fw.elf, size 30832
[ 16.209706] remoteproc remoteproc2: remote processor b004000.rtu is now up
[ 16.209732] remoteproc remoteproc3: powering up b00a000.txpru
[ 16.209880] remoteproc remoteproc3: Booting fw image ti-pruss/am65x-sr2-txpru0-prueth-fw.elf, size 36656
[ 16.209923] remoteproc remoteproc3: remote processor b00a000.txpru is now up
[ 16.235589] TI DP83867 b032400.mdio:00: attached PHY driver [TI DP83867] (mii_bus:phy_addr=b032400.mdio:00, irq=POLL)
[ 16.235874] net eth1: started
[ 16.311986] TI DP83867 46000f00.mdio:00: attached PHY driver [TI DP83867] (mii_bus:phy_addr=46000f00.mdio:00, irq=POLL)
[ 16.331112] am65-cpsw-nuss 46000000.ethernet eth0: Link is Down
[ OK ] Started Network Name Resolution.
[ OK ] Reached target Network.
[ OK ] Reached target Host and Network Name Lookups.
Starting Avahi mDNS/DNS-SD Stack...
Starting Enable and configure wl18xx bluetooth stack...
[ OK ] Started NFS status monitor for NFSv2/3 locking..
Starting Simple Network Ma…ent Protocol (SNMP) Daemon....
Starting Permit User Sessions...
[ OK ] Started Permit User Sessions.
[ OK ] Started Getty on tty1.
[ OK ] Started Getty on tty4.
[ OK ] Started Serial Getty on ttyS1.
[ OK ] Started Serial Getty on ttyS2.
[ OK ] Reached target Login Prompts.
Starting Synchronize System and HW clocks...
[ OK ] Started Enable and configure wl18xx bluetooth stack.
[FAILED] Failed to start Synchronize System and HW clocks.
See 'systemctl status sync-clocks.service' for details.
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Started Simple Network Man…ement Protocol (SNMP) Daemon..
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPLv3 packages:
autoconf
bash-dev
bash
bc
binutils
cifs-utils
coreutils-stdbuf
coreutils
cpio
cpp-symlinks
cpp
dosfstools
elfutils
g++-symlinks
g++
gawk
gcc-symlinks
gcc
gdb
gdbserver
gettext
glmark2
gstreamer1.0-libav-dev
gstreamer1.0-libav
gzip
less
libasm1
libbfd
libdw1
libelf1
libgdbm-compat4
libgdbm-dev
libgdbm6
libgettextlib
libgettextsrc
libgmp-dev
libgmp10
libgmpxx4
libidn2-0
libidn2-dev
libmpc3
libmpfr6
libreadline-dev
libreadline8
libunistring-dev
libunistring2
m4-dev
m4
make
nettle-dev
nettle
parted
pdm-anomaly-detection
python3-rfc3987
python3-strict-rfc3339
tar
which
zeromq
If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
[ OK ] Started Print notice about GPLv3 packages.
[ 19.950055] icssg-prueth icssg1-eth eth5: Link is Up - 1Gbps/Full - flow control off
[ 19.950143] IPv6: ADDRCONF(NETDEV_CHANGE): eth5: link becomes ready
[ 20.366153] icssg-prueth icssg0-eth eth1: Link is Up - 1Gbps/Full - flow control off
[ 20.366255] IPv6: ADDRCONF(NETDEV_CHANGE): eth1: link becomes ready
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org am65xx-evm ttyS2
Arago 2021.09 am65xx-evm ttyS2
am65xx-evm login: root
root@am65xx-evm:~# ethtool eth1
Settings for eth1:
Supported ports: [ TP MII ]
Supported link modes: 10baseT/Full
100baseT/Full
1000baseT/Full
Supported pause frame use: No
Supports auto-negotiation: Yes
Supported FEC modes: Not reported
Advertised link modes: 10baseT/Full
100baseT/Full
1000baseT/Full
Advertised pause frame use: No
Advertised auto-negotiation: Yes
Advertised FEC modes: Not reported
Link partner advertised link modes: 10baseT/Full
100baseT/Full
1000baseT/Full
Link partner advertised pause frame use: No
Link partner advertised auto-negotiation: Yes
Link partner advertised FEC modes: Not reported
Speed: 1000Mb/s
Duplex: Full
Auto-negotiation: on
master-slave cfg: preferred slave
master-slave status: slave
Port: Twisted Pair
PHYAD: 0
Transceiver: external
MDI-X: Unknown
Current message level: 0x00007fff (32767)
drv probe link timer ifdown ifup rx_err tx_err tx_queued intr tx_done rx_status pktdata hw wol
Link detected: yes
root@am65xx-evm:~# ethtool eth5
Settings for eth5:
Supported ports: [ TP MII ]
Supported link modes: 10baseT/Full
100baseT/Full
1000baseT/Full
Supported pause frame use: No
Supports auto-negotiation: Yes
Supported FEC modes: Not reported
Advertised link modes: 10baseT/Full
100baseT/Full
1000baseT/Full
Advertised pause frame use: No
Advertised auto-negotiation: Yes
Advertised FEC modes: Not reported
Link partner advertised link modes: 10baseT/Full
100baseT/Full
1000baseT/Full
Link partner advertised pause frame use: No
Link partner advertised auto-negotiation: Yes
Link partner advertised FEC modes: Not reported
Speed: 1000Mb/s
Duplex: Full
Auto-negotiation: on
master-slave cfg: preferred slave
master-slave status: master
Port: Twisted Pair
PHYAD: 0
Transceiver: external
MDI-X: Unknown
Current message level: 0x00007fff (32767)
drv probe link timer ifdown ifup rx_err tx_err tx_queued intr tx_done rx_status pktdata hw wol
Link detected: yes
root@am65xx-evm:~# ethtool -s eth1 speed 1000 duplex full autoneg on
root@am65xx-evm:~# [ 62.225643] icssg-prueth icssg0-eth eth1: Link is Down
[ 62.957599] icssg-prueth icssg1-eth eth5: Link is Down
root@am65xx-evm:~# sleep 30
root@am65xx-evm:~# [ 136.672549] Initializing XFRM netlink socket
[ 139.093189] process 'docker/tmp/qemu-check206201491/check' started with executable stack
root@am65xx-evm:~# ethtool eth1
Settings for eth1:
Supported ports: [ TP MII ]
Supported link modes: 10baseT/Full
100baseT/Full
1000baseT/Full
Supported pause frame use: No
Supports auto-negotiation: Yes
Supported FEC modes: Not reported
Advertised link modes: 1000baseT/Full
Advertised pause frame use: No
Advertised auto-negotiation: Yes
Advertised FEC modes: Not reported
Speed: 10Mb/s
Duplex: Half
Auto-negotiation: on
master-slave cfg: preferred slave
master-slave status: unknown
Port: Twisted Pair
PHYAD: 0
Transceiver: external
MDI-X: Unknown
Current message level: 0x00007fff (32767)
drv probe link timer ifdown ifup rx_err tx_err tx_queued intr tx_done rx_status pktdata hw wol
Link detected: no
root@am65xx-evm:~# ethtool eth5
Settings for eth5:
Supported ports: [ TP MII ]
Supported link modes: 10baseT/Full
100baseT/Full
1000baseT/Full
Supported pause frame use: No
Supports auto-negotiation: Yes
Supported FEC modes: Not reported
Advertised link modes: 10baseT/Full
100baseT/Full
1000baseT/Full
Advertised pause frame use: No
Advertised auto-negotiation: Yes
Advertised FEC modes: Not reported
Speed: 10Mb/s
Duplex: Half
Auto-negotiation: on
master-slave cfg: preferred slave
master-slave status: unknown
Port: Twisted Pair
PHYAD: 0
Transceiver: external
MDI-X: Unknown
Current message level: 0x00007fff (32767)
drv probe link timer ifdown ifup rx_err tx_err tx_queued intr tx_done rx_status pktdata hw wol
Link detected: no
root@am65xx-evm:~#
Steps to reproduce:
set SDK_VERSION=08_02_00_01
============================================================================================================================================
STEP 1.
SDK Download & Instalation for AM65x
------------------------------------
1.1 Download
Goto "">www.ti.com/.../PROCESSOR-SDK-AM65X"
click on Download options of PROCESSOR-SDK-LINUX-RT-AM65X — Linux-RT processor SDK for AM65x
click on "ti-processor-sdk-linux-rt-am65xx-evm-"$SDK_VERSION"-Linux-x86-Install.bin"
set executable permissions : chmod 777 ti-processor-sdk-linux-rt-am65xx-evm-"$SDK_VERSION"-Linux-x86-Install.bin
Execute bin file : ./ti-processor-sdk-linux-rt-am65xx-evm-"$SDK_VERSION"-Linux-x86-Install.bin
Choose Destination location : <path>
wait for completion.
============================================================================================================================================
STEP 2.
Prepare sdcard with Prebuilt Images
-----------------------------------
2.1 Connect sdcard and find device file /dev/sdx for the sdcard from lsblk or "cat /proc/mounts"
2.2 Flash Prebuilt images using below commands:
$ cd <path>/ti-processor-sdk-linux-rt-am65xx-evm-"$SDK_VERSION"/bin
$ sudo ./mksdboot.sh --sdk <path>/ti-processor-sdk-linux-rt-am65xx-evm-"$SDK_VERSION"/ --device /dev/sd<x>
$ sync
After completing, unmount Sd-card and eject.
============================================================================================================================================
STEP 3.
Test throughput eth1->eth5 on AM65x IDK
---------------------------------------
3.1 Run AM65x IDK and login as root
3.2 Connect eth1 and eth5
3.3. wait for link go up
3.4. run 'ethtool -s eth1 speed 1000 duplex full autoneg on'
3.5. wait 30 seconds
3.6. run 'ethtool eth1' and see that link is still not up