Part Number: TDA4VM
Hi Ti team
We are testing 16ch 720p 6fps encoding on TDA4VM.
If we create more than 8 Encoder instances,
The following message is output and creation is not possible.
[ 217.204145] Firmware used_socks[8] max context[8]
[ 217.210345] ERROR: Firmware context limit reached!
So, find the kernel code that outputs the message
I made the following fixes, but still can't use more than 8 encoders.
drivers/media/platform/vxe-vxd/encoder/fw_binaries/ALL_CODECS_FW_ALL_pipes_2_contexts_8_hwconfig_1_bin.c
unsigned char *all_codecs_fw_all_pipes_2_contexts_8_hwconfig_1_define_names_array[] = {
"TOPAZHP_NUM_PIPES",
"TOPAZHP_MAX_BU_SUPPORT",
"MAX_REF_B_LEVELS_FW",
"SEI_INSERTION",
"TOPAZHP_MAX_NUM_STREAMS",
};
unsigned int all_codecs_fw_all_pipes_2_contexts_8_hwconfig_1_define_values_array[] = {
2,
(TOPAZHP_MAX_BU_SUPPORT_HD),
0,
One,
16, // encoder count 8->16
};
Is what we are trying to test impossible?
Please advise on how to try this.
Thank you,
Sungnam.