Part Number: TDA4VM
I tried to use TI latest edgeai image for TDA4VM, it has some gst-plugin inside the image(although this image disabled weston, but it still works using kmssink instead of waylandsink) , test some commands from TI wiki and GitHub page, but still doesn't works as attached failed log. So I think the major problem is I don't know how to change the virtual channel number using gstreamming.
I'll appreciate if someone can give me directions, thanks a lot
root@tda4vm-sk:/opt/edge_ai_apps# gst-launch-1.0 videotestsrc is-live=true ! mux. tiovxmux name=mux ! video/x-raw,width=1280,height=800 ! tiovxdemux name=demux demux. ! queue ! kmssink APP: Init ... !!! MEM: Init ... !!! MEM: Initialized DMA HEAP (fd=4) !!! MEM: Init ... Done !!! IPC: Init ... !!! IPC: Init ... Done !!! REMOTE_SERVICE: Init ... !!! REMOTE_SERVICE: Init ... Done !!! 16416.879118 s: GTC Frequency = 200 MHz APP: Init ... Done !!! 16416.879215 s: VX_ZONE_INIT:Enabled 16416.879225 s: VX_ZONE_ERROR:Enabled 16416.879230 s: VX_ZONE_WARNING:Enabled 16416.879736 s: VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!! 16416.880002 s: VX_ZONE_INIT:[tivxHostInitLocal:86] Initialization Done for HOST !!! WARNING: erroneous pipeline: could not link mux to demux, mux can't handle caps video/x-raw, width=(int)1280, height=(int)800