Part Number: SK-AM64
Dear TI Engineers,
I have a AM64x Starter Kit and I can configure it to work according to Wi-SUN wfantund user guide.
- My next step is to create applications. The original documents do not have any information about creating applications. Please show me some official information about creating applications on AM64x Starter Kit.
https://software-dl.ti.com/processor-sdk-linux/esd/AM64X/08_02_00_17/exports/docs/devices/AM64X/index_Applications.html - According to the user manual of AM64x Starter Kit, the Raspberry Pi extension header provides a maximum of 200mA current. If I install a very hard-working broad band dialup modem which may exceed 200mA usage, is it possible to increase the Raspberry Pi extension bus's current supply?
Yours faithfully,
Timmy