Other Parts Discussed in Thread: OMAP-L138, TPS65070, SYSBIOS
Hello,
I am experimenting with the omap-l138, and I would like to run an audio application from the screen.
As a first step, I try to launch the biospsp audio example provided with SDK and, in the same time, the matrix-gui-e is on but I get some troubles. Twice are working well separately, however when I run them together I get the error message "tps6507x 1-0048: TSC mode read failed".
It seems that this issue comes when initializing the codec aic3106. But I am not sure what causes the problem, could it be a bad i2c initialization issue? Would it due to a competitive use of i2c bus?
Thanks in advance