Part Number: TDA4VM
Is it possible to generate two different formats from LDC once for the same input: 420 & 422?
In the TRM it is mentioned "Dual output channels for programmable output pixel size" Does this has any relation to what i asked?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VM
Is it possible to generate two different formats from LDC once for the same input: 420 & 422?
In the TRM it is mentioned "Dual output channels for programmable output pixel size" Does this has any relation to what i asked?
No the output format cannot be different for dual output. 8bit output is just from 12bit output, by doing bit depth conversion. There is no format conversion.
Regards,
Brijesh
Continuing to the same,
Is it possible to have only lens distortion in one output. Lens distortion + Affine transform in one output. Can it be configured in such a model?
No, the only difference between output is bit depth. Otherwise they are identical.