Part Number: AM6442
Hello at TI experts!
I wonder if the MMC1 controller of the AM6442 support Wifi SDIO devices (hardware and software question of course !)
Im' trying to use such device on TMDS64GPEVM and Sk-AM64 board : both have SDCard slot on MMC1 and I'm using this slot to connect a SDIO Wifi controller. I don't manage to get it working, it usually don't pass the initialization stage.
I'm asking this question because I know MMC0 for example is not compatible with SDIO (see datasheet and also https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1031005/am6442-mmc0-and-mmc1-supported-modes), and would like to have the details about MMC1 features on this specific topic.
Note: SK-AM64 has Wifi SDIO device on MMC0 so I really wonder about the specifications, this is supposed to not work on this board !!! The datasheet clearly indicates SDIO is NOT supported on MMC0.
Thanks,
Joel