This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM64X: EtherCAT Slave Sync1 generated too late

Part Number: PROCESSOR-SDK-AM64X

Dear TI team,

we're seeing an issue with the EtherCAT slave firmware where the Sync1 pulse is being generated one Sync0 period too late.

In our use-case we're configuring the Sync1 cycle time to be a multiple of the Sync0 cycle time. We haven't looked at the behavior of the TIESC slave when Sync1 is simply shifted from Sync0.

For our test case we've configured the system for 1ms Sync0 cycle time and 5ms Sync1 cycle time.

We've instrumented execution of the Sync0/Sync1 ISRs and tasks to make sure we're not just being scheduled too late. We can see that the Sync1 task executes within a few microseconds (5-12) after the Sync1 ISR. If we look at the Sync0/Sync1 events beginning with the first Sync0 event, we see the following sequence.

ts (us) systime (us) NextSync0 (us) NextSync1 (us)
0 11.4 Sync 0 task 0.0 986.7
1 1002.9 Sync 0 task 992.1 986.7
2 2003.8 Sync 0 task 1992.9 1986.7
3 3001.8 Sync 0 task 2991.1 2986.7
4 4006.9 Sync 0 task 3996.0 3986.7
5 5015.6 Sync 1 task 5004.3 8986.7
6 5022.8 Sync 0 task 5012.1 5986.7
7 6002.8 Sync 0 task 5992.0 5986.7
8 7003.0 Sync 0 task 6992.2 6986.7
9 8001.9 Sync 0 task 7991.1 7986.7
10 9005.6 Sync 0 task 8994.8 8986.7
11 10011.9 Sync 0 task 10000.2 10986.7
12 10017.2 Sync 1 task 10006.3 13986.7
13 11002.2 Sync 0 task 10991.1 10986.7
14 12001.9 Sync 0 task 11990.9 11986.7

(ts in us is based on the R5f cycle counter, systime is read via bsp_get_local_sys_time, NextSync0/NextSync1 are read from ESC_ADDR_NEXT_SYNC0/1_PULSE)

(systime, NextSync0 and NextSync1 are relative to the first systime we've logged, so that the numbers are easier to read)

  • The first Sync1 Event is generated together with the 6th Sync0 Event, instead of with the 5th Sync0 Event. The period is ok.
  • The NextSync0 timestamps are sometimes not yet updated when we read them (marked in light blue). This is due to PINDSW-2360. We can work around that.
  • In line 5, the NextSync1 register reads ~9ms. At that moment the systime register shows ~5ms. If we take the "NextSync1" value of 9 ms, and subtract the period of 5ms, we see that this event SHOULD have fired at 4ms. This shows how the Sync1 event fires one Sync0 period too late.
  • In line 12, we see that the second Sync1 event fired at ~10ms. If we take "NextSync1" value of ~14ms and subtract the period of 5ms, we see that this event SHOULD have fired at 9ms, which is also what NextSync1 showed back in line 5.
  • We've also tested with other Sync0/Sync1 cycle times, and so far it's been always one Sync0 period that the Sync1 was being generated too late.

It seems that this is a bug within the TIESC firmware. We can work around this, but of course it would be nice to have this a) confirmed by TI and b) eventually fixed.

We've seen this bug in MCU+ SDKs 08.00 (slave firmware 5.4.242) , 08.02 (slave firmware 6.5.0) and 08.03RC1 (slave firmware 6.5.2).

Let me know if you need any further details regarding this issue.

Best Regards,

Dominic