Part Number: TDA4VM
Other Parts Discussed in Thread: AWR2243
Hi,experts
Recently, I am studying how to use CSI RX interface to receive AWR2243 data.
As the relevant hardware is not ready yet, I am now doing some pre research work and hope to get some suggestions from you. Here is my description:
I noticed that there are several examples of cameras in the SDK, but the connection method used in these examples is FPD link.
The way I use is that AWR2243 is directly connected with CSI RX interface, that is, there is no ub960 and ub953.
My question is:
1. Does Ti provide examples of CSI RX using direct connection? If so, can you provide them?
2. If the answer to question 1 is no, I think the following example can be modified to meet my requirement:
ti-processor-sdk-rtos-j721e-evm-08_01_00_11/pdk_jacinto_08_01_00_33/packages/ti/drv/csirx/examples/csirx_capture_test/src/csirx_capture_test_main.c
In this example, do I need to pay attention to anything other than removing the code of ub960 and I2C?
Appendix: My SDK version is ti-processor-sdk-rtos-j721e-evm-08_01_00_11
Best Regards,
Tao