Part Number: TMDSICE3359
Hi Team,
I am new to the etherCAT domain. For my new project I have to setup an etherCAT master slave communication. Following are my doubts regarding this implementation,
- I have seen a document for EtherCAT Master deign, is there is any documentation available for EtherCAT Slave design?
- Can I use the one TMDSICE3359 board as the master and one other TMDSICE3359 board as a slave in the setup? if it can't be used then why?
- Do I get linux support on this board?
- Is there is any documentation or tutorial from TI on EtherCAT protocol available as of now?
- Is there is any other EVM from TI that supports EtherCAT communication and two RJ45 connectors on it?
Regards,
Vineeth