Hi,
I am starting to use the following C55x variants: C5510A, C5505, C5504
Question on C5510A:
- Is this processor the same as the C5510 v2.2?
- If yes, does that mean I can use the same CSL macro (CHIP_C5510PG2_2) and CSL library csl5510PG2_2x.lib?
- If no, how do I get the CSL library for this? I am using CCS 3.3 SR12 (I cannot move to CCS 4 yet)
Question on C5505, C5504:
- How do I get the CSL libraries for these? I am using CCS 3.3 SR12 (I cannot move to CCS 4 yet)
Thanks,
MA