This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: TIDL delegate with multiple subgraphs

Part Number: TDA4VM


Hi, 

According to https://software-dl.ti.com/jacinto7/esd/processor-sdk-rtos-jacinto7/08_02_00_05/exports/docs/tidl_j721e_08_02_00_11/ti_dl/docs/user_guide_html/md_tidl_fsg_quantization.html , we should be using floating point model as input. If there are multiple subgraphs, I believe the ones offloaded to C7x would be in fixed point. What about the parts of the model which are running on ARM - would they be in floating point or fixed point? If this is in floating point, would you advise to use a quantized tflite model as input?

Thanks.

Kind regards,

Sharon