Hi,
I have C5505 eZDSP USB Stick Development Tool and install CCS4 version coming with it.
I did obtain a licence for it online (register using the activation code), installed it and all works fine.
Now I want to use CCS4 for MSP430 development. When I tried to flash a sample code into eZ430-F2013 I have an error:
'You are not licensed to use the currently configured connection-type'
So I did registration again, but the new file doesn't work either, giving another error.
What to do to have licenses for both kits eZDSP and eZ430?
How can I display/read what is the licence type that I have (or rather theCCS4 allows me to use)?
Jan