This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM:Issue in running custom layer on target

Hi 

We are trying to implement a custom layer which works fine during Importing and PC Emulation.Please find the details of  last five  layers after importing

68|TIDL_ConvolutionLayer |576 | 0| 1| 1| 64 x x x x x x x | 68 | 1 320 16 16 | 1 256 16 16 | 21102592 |
69|TIDL_ConcatLayer |577 | 0| 4| 1| 65 66 67 68 x x x x | 69 | 1 256 16 16 | 1 1024 16 16 | 262144 |
70|TIDL_ConvolutionLayer |580 | 0| 1| 1| 69 x x x x x x x | 70 | 1 1024 16 16 | 1 256 16 16 | 67239936 |
71|TIDL_CustomLayer |590 | 0| 1| 1| 70 x x x x x x x | 71 | 1 256 16 16 | 1 256 32 32 | 1048576 |
72|TIDL_DataLayer |590 | 0| 1| -1| 71 x x x x x x x | 0 | 1 256 32 32 | 0 0 0 0 | 0 |

But the results on target are not as expected.
We have build tidl using make rt and TI_DEVICE_a72_test_dl_algo_host_rt.out was generated.

We are also not able to dump layerwise outputs from target with debugtracelevel=1 and writetracelevel=3.
PFA the logs:

[C7x_1 ] 69.951423 s: 0 1.00000 0.00000 255.00000 0
[ 130.996498] Initializing XFRM netlink socket
[ 133.106569] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
[ 133.124820] Bridge firewalling registered
[MCU2_0] 187.719442 s: DHCP client timed out. Retrying.....
[MCU2_0] 355.719440 s: DHCP client timed out. Retrying.....
[MCU2_0] 523.719443 s: DHCP client timed out. Retrying....

How to get layer dumps from target?

During inference we are using execmode  "TIDL_EXEC_MODE_INFER_PROCESS_REF".Is this mode expected to run on target too?

NOTE: SDK used : ti-processor-sdk-rtos-j721e-evm-07_01_00_11

Regards

Vyom MIshra