This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: J784S4X - PCIE signal and lanes usage

Part Number: TDA4VM

As per note 9, page 8 in DM, TDA4xH supports 1x4L or 2x2L option but Table 5-1 shows TDA4xH supports 2x4L or 4x2L options ?

  We have considered as per note 9 and used 2x2L PCIE option, and the following signals are considered;

  – PCIE0 Lane 0 and Lane 1

  – PCIE1 Lane 0 and Lane 1

  Please confirm the same.

Reference Schematic: J784S4X Evaluation Board
Rev: E2
Ver: 3.1
File Name: PROC141E2(001)_SCH
Reference: DM- Note 9 (Page 8) and Table 5-1 (Page 7)