This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Kernel would not finish uncompressing

I have the DM365 and I loaded this new kernel with some modifications, on the board-dm365-evm.c

everything compiles fine but the kernel would not load,  any ideas what it could be?

 

NAND read: device 0 offset 0x1000000, size 0x1b00000                           
 28311552 bytes read: OK                                                       
                                                                               
Loading from NAND 256MiB 3,3V 8-bit, offset 0x400000                           
   Image Name:   Linux-2.6.32.17-davinci1                                      
   Image Type:   ARM Linux Kernel Image (uncompressed)                         
   Data Size:    2145592 Bytes =  2 MB                                         
   Load Address: 80008000                                                      
   Entry Point:  80008000                                                      
## Booting kernel from Legacy Image at 80700000 ...                            
   Image Name:   Linux-2.6.32.17-davinci1                                      
   Image Type:   ARM Linux Kernel Image (uncompressed)                         
   Data Size:    2145592 Bytes =  2 MB                                         
   Load Address: 80008000                                                      
   Entry Point:  80008000                                                      
   Verifying Checksum ... OK                                                   
   Loading Kernel Image ... OK                                                 
OK                                                                             
                                                                               
Starting kernel ...                                                            
                                                                               
Uncompressing Linux.............................................................