Other Parts Discussed in Thread: OMAP3530
Hi:
I used the OMAP3530 and the develop env is dvsdk_3_00_02_44, and CCS4.0
I want to added a codec(such as mp3) into the code engine. I have finished the audio codec (source code,such as mp3) in the CCS4 ( It can decode ) .
And I have Successfully run the videocopy demo in board (OPMAP3530) . Then I want to add the audio codec in CE and run in board.
How should I do now ?
I am a new user
Waiting for your help.
Thanks a lot!!!