Part Number: D3-3P-TDA3X-SK
Other Parts Discussed in Thread: DS90UB953-Q1, DS90UB935-Q1
I'm attempting to display YUV-422 8-Bit CSI-2 video on the D3-3P-TDA3X over FPD-link III, vision SDK 3.06. While the serializer (UB935) appears to be sending valid YUV-422/8-bit, the RX_PORT_STS2 Register (Address 0x4E) on the UB960 is reporting buffer errors. According to the UB960, the line length on he video appears to be correct. We are able to display RGB888 video (using the pattern generator) but not YUV-422/8 with the same hardware.
What might cause the Buffer Error bit in the UB960 (reg 0x4E) to be set in the YUV422 case?
Thanks.