Hello All
I have been using DM648 EVM from lyrtech from quite sometime. I developed several application using NDK, Ethernet and PCI interface. I want to interface a camera with my board and then loopback the realtime video out from the board. I also want to see the packets in the DSP memory. I used the application which comes with BSL in Lyrtech folder but even in video loopback project it only shows color bars. Someone suggested me to use CSL in DVSDK 1.1 but those applications fail to build plus also I think they are Linux based, I want to do it on Microsoft Windows anyone there to help?