Part Number: AM5708
Other Parts Discussed in Thread: AM5728
Hello.
I am using AM5708 board and CortexA15_0 core.
I'd like to make an SD card for booting that fits above, but I have the following question.
I entered the following in Windows CMD when I made the SD card boot program for AM5728:
MulticoreImageGen.exe LE 55 C:\Users\app 0 C:\Users\rprc.rprc
The SBL User Guide TDA states:

When I create the SD card boot program for AM5708, I wonder which value should I put in the above sentence for LE (ENDIAN) and 55 (Dev Id).
I also want to know the location of the document with the corresponding information.