Other Parts Discussed in Thread: OMAP-L137, SYSBIOS
Hello,
I'm using CCS 4.2.3 to develop an application using SYS/BIOS (6.31) and CSLr for the OMAP-L137/C6747. The application is made up of an RTSC configuration project and a C project. The C project uses the #include <tistdtypes.h> for CSLr and #include <xdc/std.h> for RTSC/XDC. But these two header files have some typedef statements that declare types with the same names, for example Int8, Uint8, etc. This situation causes build errors like:
""Int8" has already been declared in the current scope C:/Work/ti/xdctools_3_20_08_88/packages/xdc std.h line 206"
I don't know how I can avoid including <xdc/std.h> and the other xdc and sysbios headers because the C project requires knowledge of the xdc and sysbios structures and functions.
What am I doing wrong?
Thanks,
SC