This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

migration the NDK Protocol stack of TMS320C6678 and use the order of ping is failed



1. four package are shown below:

PDK_C6678_1_1_2_6;

ndk_2_21_01_38,

bios_6_33_06_50,

mcsdk_2_01_02_06

2.

examples of using the path that "mcsdk_2_01_02_06/examples/ndk/client" and compiler is successful,

connected PC computer can be recognized,but ping is failed

3.

please ask if the question of the driver? example ethdriver.c、csl_emac.c、nimu_eth.c ,Do you encounter similar problems and how to solve them,thanks very much!