Other Parts Discussed in Thread: TMS320VC5501
If I wanted to boot the 5501 via the SPI EEPROM Boot Mode; is there an application that would allow me to actually program the SPI EEPROM with the run-time code through the 5501? I don't want to program the EEPROM before mounting it to the board; and I don't want to add isolation circuitry to isolate the EEPROM if I need to upgrade my code. I'm planning to incorporate a JTAG interface and I am hoping there is a way to use the JTAG port to get my application code into the EEPROM.