Hi,
I'm using the spreadsheet to get an idea of power consumption. Most of it make sense with the exception of the the DSP option and the ARM MM.
For the DSP there are three options - Disabled, Megamodule sleep mode and enabled. The question I have is what's the difference between having the megamodule sleep mode and the enable mode? and how does it relate to utilization?
If I have the device in megamodule sleep mode and have 20% utilization what's the difference between that and active mode and 20% utilization? In one mode does the spreadsheet assume that when not being utilized then you are in sleep mode?
For the ARM MM there are 4 modes - is there a typical rule of thumb as to the difference between Low, Medium and high activity? - does this really relate to the OS and the amount of time is is waiting for something versus the OS firing off tasks?
Thanks
Calum