Part Number: TMS320C6657
I wonder theoritically which flash boots faster if NAND flash or NOR flash are used as direct boot device without IBL?
Of course,the same chips as the EVM6657 board used are applied to boot C6657.
Thank you for your help!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320C6657
I wonder theoritically which flash boots faster if NAND flash or NOR flash are used as direct boot device without IBL?
Of course,the same chips as the EVM6657 board used are applied to boot C6657.
Thank you for your help!
Hi,
This question relates to the ROM, I will start by checking the TRM to see if this timing is documented.
Will come back to you shortly.
I wonder theoritically which flash boots faster if NAND flash or NOR flash are used as direct boot device without IBL?
Of course,the same chips as the EVM6657 board used are applied to boot C6657.
Without IBL, theoretically, NAND flash will be the faster one than the NOR FLASH. Because, the NAND is interfaced through EMIF 16 and the NOR is through the SPI.
You can literally imagine the speed difference between the serial transfer ( SPI- NOR) and the parallel transfer (EMIF-NAND).
--
Additionally, that's why the IBL plays a vital role in configuring the PLL clock to speed up the peripherals such as NOR,NAND etc...
Regards
Shankari G