Part Number: TDA4VM
Hi expers,
I try to monitor voltage by pok, during the test, it was found that the MMR register could not be written
eg: try write CTRLMMR_WKUP_POK_VDDR_CORE_UV_CTRL (0x4301811C) POK_TRIM field to 0x50 as follow:
pr_info ("pok config start0 0x%x\n", CSL_REG32_RD (0x4301811C));
CSL_REG32_WR (0x4301811C, 0x80000050);
pr_info ("pok config start1 0x%x\n", CSL_REG32_RD (0x4301811C));
however the value of CTRLMMR_WKUP_POK_VDDR_CORE_UV_CTRL register is always 0x80000014, output as follow:
sdr-pok: pok config start0 0x80000014
sdr-pok: pok config start1 0x80000014
Using CSL POK example, I can not recvice any esm error interupt.
Regards,
Li quan