Other Parts Discussed in Thread: TCA6424A
Hi,
We have multiple J721 SoM Board and custom baseboards.
With the latest Revision PROC078A we noticed different behaviors. On the Standard Baseboard (J721EXCP01EVM) all Revisions are working as expected.
Also the older (PROC078E7A and PROC078E8A) revisions are working without any problems with our baseboard.
We tried from SDK 07.03. up to SDK 08.01.(what is shipped with the SoM board)
Most of the time on the first start up the latest revision of the SoM board is booting completely on "our" baseboard.
But hard resetting or via command: "reboot" the boot process will stop at a random time.
At that "stopped" state, all PMIC A and PMIC B output voltages are off.
I also tried to lower the DDR Frequency like in that post: e2e.ti.com/.../faq-tda4vm-on-7-3-8-0-sdk-how-to-reduce-ddr-speed-to-3733-mts
Any further advise / approach?
Thank you