Part Number: TMS320C5504
Hi Experts,
Good day. Seeking assistance on this query:
The "10" grade of the "TMS320C5504AZCH" has a spec of a core voltage of 1.3V and a maximum clock speed of 100MHz, but is it possible to run at a maximum 100MHz clock speed?
For example, is there a recommendation to keep it below 95% etc.? Even if 100MHz clock operation is not a problem, the frequency of the primary oscillator connected to the external of DSP IC also has a tolerance, so even if the internal PLL uprates the frequency to 100MHz, the tolerance will still have an effect.
Please let us know the allowable tolerance of 100MHz clock. Thank you.
Regards,
Archie A.