This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Too much noise in Leads of ECG

hi,

Actually i am doing project of implementing ECG on c5505. Now  i am successfully connected to the pc. but i am again stuck . there are two things i wanted to know that i have set up all the connections as given on the guide, what do i do next??? should i need to write code on CCS or used the given ".out" file with th EVM and the guide mentions "ecgsystem.pjt" but its not here in cds given. i use "ecgsystem-nonbios.pjt" which is given actually , the lcd and pc application starts to give signals but they all are too much noisy.

Secondly if i use the .out file then there is much noise...

so can u advice me how to proceed further... It would be a great help again.