Other Parts Discussed in Thread: AM5718
Hello, experts.
I want to boot through RTOS-based SBL on AM5708.
The questions are as follows:
When attempting to boot through AM5708, which of the following is possible?
1. Booting Via eMMC
2. Booting Via QSPI
3. Booting Via SD Card
The above question is because the AM5718 IDKEVM, which we know is similar to the AM5708, supports two of the three (QSPI, SD Card) SBL boot modes.