This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSS and Camera ISP Clock Synchronisation

Is it possible to synchronise the DSS clock to the Camera ISP clock?

I am using a SD video camera as input to the CCDC/ISP and displaying the video on a TV monitor using the composite interface. Since the input and output are not synchronised, I notice a problem with the ISP capture running out of buffers. Ultimately, the application will have to drop frames, which is not ideal and so synchronising the clocks will avoid this completely. Is there a way to do this?

Thanks,

 

Andy