Using DM816x, I want to show video on the LCD panel(RGB565/RGB888) using VOUT1 port, and show the same content through HDMI(on chip) simultaneously.
Question 1:
I wonder if the VOUT1 port supports the RGB888 mode? If not, how can I implement the requirment (VOUT1->RGB565/RGB888).
Question 2:
Because the resolution of my LCD panel is low (320*272), I' m not sure if the conent can be shown using VOUT1(LCD) and using HDMI simultaneously
Thank you for your suggestion in advance.