Hey all,
I have a c5505 ezDSP stick, and I am having an issue with the audio output. I was developing some code for the device and left it one evening in a working state, I then came back to it the next morning and did nothing to the code. I did however carefully attach the board to a plastic lid for a box (to house the device for protection...), and after powering it back up again the audio ouput of the device is massively reduced. I have loaded in the audio filter example to test whether it is my code, but that produces the same low output. Have I somehow blown the codec? Or has it got itself somehow locked into a low volume state?
J