This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS243GPEVM: EnDat example - change PRU1 to PRU0

Part Number: TMDS243GPEVM

Dear all,

currently I am working on the EnDat example, taken from the "AM243x MCU+ SDK 08.01.00". The example is build for PRU1 channel0. I've managed to get it work, however i want to change the PRU used from PRU1 to PRU0.

- What changes need to be done to do so?

I've tried to edit the makefile and build a new PRU firmware, changed the PRU instance in the example.syscfg and edited the config and control register base addresses. I haven't made it work yet. Am I missing something here?

Thanks!

Best regards,

Jan