This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

File System for SD-CARD

I am using a C5504 DSP for my application and have a SD-CARD interfaced to it.

I would like to know if TI provides any thin file system for the same. So that i can directly use it store my data on the SD-CARD.

 

Thanks

 

  • Ankush,

    If you are looking simply to use SD card as external storage then you could look at the Chip Support Library (CSL) which contains low level code for controlling / communicating with DSP peripherals.  The CSL for the C5504 is currently in beta and should be released before the end of this quarter.  In preparation you can start using the CSL which is currently available which supports all C5500 prior to C5504/C5505.  You can then migrate to C5504 version when it becomes available.

    If you are looking for something like FAT file system support, then there are a number of TI Third Party providers that can provide this type of product for C5500 DSPs.  You can find suppliers by searching for File System from this page: http://focus.ti.com/dsp/docs/thirdparty/catalog/searchcatalog.tsp.