Hi
Please if somebody have a ECGSystem_V_5_0 and SpO2System_V_5_0 Project source code, please send to me I nedd very much
leandromestree@gmail.com
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The project source code is delivered with the ECG and SpO2 Analog Front End modules for the C5505 Medical Development Kits. Here are links for the EVM and AFEs:
http://focus.ti.com/docs/toolsw/folders/print/tmdxevm5505.html
http://focus.ti.com/docs/toolsw/folders/print/tmdxmdkek1258.html
http://focus.ti.com/docs/toolsw/folders/print/tmdxmdkpo8328.html
Hi TommyG,
Our company is using the EVM5505 and Pulseoximeter Front End module, however i cannot find sufficient information in the CD. In side the CD there are just two file: 1) C550X_MD.exe and 2) MDK_PULS.pdf. I really cannot find the information as descrip in the table 2. Could you please send me the follow information to me? The project schedule is very tight, please help.
My company email is alantso@automatic.com.hk or hotmail: alantso2003@hotmail.com
Thank you for your attention
Regards,
Alan
S Number Directory/Filename Contains
1 SpO2System_V_5_0 Project source code
2 Output Contains three files:
SpO2System.out
c5505evm.gel and
VC5505 XDS510USB Emulator.ccs
3 PCApplication Executable for PC application
4 BootImageCreation.zip Folder that contains the following files:
bootImage.exe
convertBind0.bat
convertEnc0.bat
convertInsecure.bat
programmer.out
readme.txt
5 Document Contains the following documents:
ReleaseNote.txt
Quick starter guide V6.0 doc