Part Number: AM5728
Hi,
Is it possible to define the cache size under the bare metal of the A15 side, I did not find the API in the PDK, like CACHE_setL2Size under C6000?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM5728
Hi,
Is it possible to define the cache size under the bare metal of the A15 side, I did not find the API in the PDK, like CACHE_setL2Size under C6000?
Hi Nancy,
I don't think that it is possible.
Can you please tell what is your use case here?
Regards,
Parth
Hi,
Can you please tell what is your use case here?
Customer defines the Ethernet sending and receiving data structure and array. When the data is defined in OCM1--3, the data can be sent and received normally. When these data are defined in the DDR space, the data cannot be sent and received normally. Guess it may be related to cache.
After comment the CSL_A15_INIT_startup in pdk_am57xx_1_0_18\packages\ti\csl\arch\a15\src\csl_a15_startup.c, which is equivalent to not opening the cache and MMU, and then assigning the data to the DDR , and the Ethernet can work normally.
Hi Nancy,
When these data are defined in the DDR space, the data cannot be sent and received normally. Guess it may be related to cache.
What do you mean by data cannot be sent and received normally? What are the error you are facing with assigning data to DDR space?
Regards,
Parth
Hi Parth
data cannot be sent and received normally ,that means is that:when sending and receiving data structure and array defines in DDR,data write to sending data array,actually data cannot tramsmit out from sending array.also when other device through ethernet send data to my device,there is actually no data in the receive data array. However when sending and receiving data structure and array defines in OCM1--3 area sent and receive all normally.DDR and OCM differ in DDR enable cache already.if disable DDR cache function and sending and receiving data structure and array defines in DDR again,receive and send all normally