Hi,
We are developing DM365 based hardwaer/software solution.
On the initial phase of our project, we developed application using NFS.
We are trying to put everything on the file system. We are using arago base file system from PSP download page.
Please help me with the following queries.
1. We are not able to figure out where should we put our application in the start up of file system (Arago base demo file system )
2. We tried to put our application in /etc/init.d/bootmisc.sh. But as such our application is using serial port 0, the application is flooded with random data on the serial port (PS: we have disabled the serial port console from kernel boot argument and in the file system /etc/inittab )
We are using open source kernel from git linux-2.6.32 from GIT.
Thanks & Regards,
Jagdish