Part Number: AM6548
Hi experts
We encounter a problem, when plug or unplug the cable, it would show some error information:
icssg0-eth eth0 Link is up - 1Gbps/full - flow control off
icssg0-eth eth0: timeout waiting for command done
then the ethernet port can not work normally, it can not send or capture the packets it can not get the dynamic ip address.
even if we assign a static ip address, it also can not ping with each other.
can you help to figure out what's wrong?