This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI-SCI client driver

Hi, 

I'm working on the TI-SDK-08_01_00_07 on a J721e based board. We were planning to use ti-sci firmware in the Linux kernel coming as part of this SDK. However, on investigation, it has been observed that, the ti_sci.c -- which is loaded as an in-built platform driver in Kernel is slightly out-dated when compared to its counter-part in u-boot or ti-spl.bin. It lacks support for some of the "Processor Control Messages" like: TISCI_MSG_PROC_AUTH_BOOT_IMIAGE, TISCI_MSG_WAIT_PROC_BOOT_STATUS. Is there a plan to update the ti-sci.c driver in the kernel updated? If it is already done, can the same be shared? 

Also, another follow-up question is that, if the sysfw functionality has to be invoked by an application running on Linux, is there a utility or library developed by TI to use the same. 

Expecting a quicker response.

Thanks,

Srivatsan