I follow this instructions http://processors.wiki.ti.com/index.php/DMAI_GStreamer_Plug-In_Getting_Started_Guide top get gstreamer in the file system using Ubuntu 9.10
after typing this command:
make DVSDK_INSTALL_DIR=$HOME/dvsdk/dvsdk_3_10_00_19 TARGET_ROOT_DIR=$HOME/install/dm365_fs PLATFORM=dm365 all install
I get this errors, was anyone able to compile GStreamer?
is this guide outdated or am I using the wrong version?
CC gstosssink.o
CC gstosssrc.o
LINK libgstossaudio.la
make[4]: Leaving directory `/home/icemetal/gst-ti-plugin-full-1.02.00/opensource_build/gst-plugins-good-0.10.16/sys/oss'
***** building plugins_good (sys/v4l2)
make[4]: Entering directory `/home/icemetal/gst-ti-plugin-full-1.02.00/opensource_build/gst-plugins-good-0.10.16/sys/v4l2'
CC gstv4l2.o
cc1: warning: include location "/usr/include" is unsafe for cross-compilation
CC gstv4l2colorbalance.o
cc1: warning: include location "/usr/include" is unsafe for cross-compilation
CC gstv4l2object.o
cc1: warning: include location "/usr/include" is unsafe for cross-compilation
CC gstv4l2bufferpool.o
cc1: warning: include location "/usr/include" is unsafe for cross-compilation
CC gstv4l2src.o
cc1: warning: include location "/usr/include" is unsafe for cross-compilation
CC gstv4l2sink.o
cc1: warning: include location "/usr/include" is unsafe for cross-compilation
CC gstv4l2tuner.o
cc1: warning: include location "/usr/include" is unsafe for cross-compilation
CC gstv4l2vidorient.o
cc1: warning: include location "/usr/include" is unsafe for cross-compilation
CC v4l2_calls.o
cc1: warning: include location "/usr/include" is unsafe for cross-compilation
CC v4l2_dm365_ipipe.o
cc1: warning: include location "/usr/include" is unsafe for cross-compilation
v4l2_dm365_ipipe.c:70:41: error: media/davinci/imp_previewer.h: No such file or directory
v4l2_dm365_ipipe.c:71:39: error: media/davinci/imp_resizer.h: No such file or directory
v4l2_dm365_ipipe.c:72:39: error: media/davinci/dm365_ipipe.h: No such file or directory
v4l2_dm365_ipipe.c: In function 'gst_v4l2_dm365_resizer_init':
v4l2_dm365_ipipe.c:182: error: 'IMP_MODE_CONTINUOUS' undeclared (first use in this function)
v4l2_dm365_ipipe.c:182: error: (Each undeclared identifier is reported only once
v4l2_dm365_ipipe.c:182: error: for each function it appears in.)
v4l2_dm365_ipipe.c:185: error: storage size of 'rsz_chan_config' isn't known
v4l2_dm365_ipipe.c:186: error: storage size of 'rsz_cont_config' isn't known
v4l2_dm365_ipipe.c:193: error: 'RSZ_S_OPER_MODE' undeclared (first use in this function)
v4l2_dm365_ipipe.c:195: error: 'RSZ_G_OPER_MODE' undeclared (first use in this function)
v4l2_dm365_ipipe.c:207: error: 'RSZ_S_CONFIG' undeclared (first use in this function)
v4l2_dm365_ipipe.c:217: error: 'RSZ_G_CONFIG' undeclared (first use in this function)
v4l2_dm365_ipipe.c:186: warning: unused variable 'rsz_cont_config'
v4l2_dm365_ipipe.c:185: warning: unused variable 'rsz_chan_config'
v4l2_dm365_ipipe.c: In function 'gst_v4l2_dm365_previewer_init':
v4l2_dm365_ipipe.c:340: error: 'IMP_MODE_CONTINUOUS' undeclared (first use in this function)
v4l2_dm365_ipipe.c:343: error: storage size of 'prev_chan_config' isn't known
v4l2_dm365_ipipe.c:350: error: 'PREV_S_OPER_MODE' undeclared (first use in this function)
v4l2_dm365_ipipe.c:352: error: 'PREV_G_OPER_MODE' undeclared (first use in this function)
v4l2_dm365_ipipe.c:363: error: 'PREV_S_CONFIG' undeclared (first use in this function)
v4l2_dm365_ipipe.c:343: warning: unused variable 'prev_chan_config'
make[4]: *** [libgstvideo4linux2_la-v4l2_dm365_ipipe.lo] Error 1
make[4]: Leaving directory `/home/icemetal/gst-ti-plugin-full-1.02.00/opensource_build/gst-plugins-good-0.10.16/sys/v4l2'
make[3]: *** [plugins_good.build] Error 255
make[3]: Leaving directory `/home/icemetal/gst-ti-plugin-full-1.02.00/opensource_build'
make[2]: *** [.plugins] Error 2
make[2]: Leaving directory `/home/icemetal/gst-ti-plugin-full-1.02.00/opensource_build'
make[1]: *** [opensource_build] Error 2
make[1]: Leaving directory `/home/icemetal/gst-ti-plugin-full-1.02.00'
make: *** [all] Error 2
icemetal@ubuntu:~/gst-ti-plugin-full-1.02.00$