Hi,
[Question1]
Is there a difference in performance between USB0 and USB1?
I confirmed that there is a restriction that only USB0 can be selected with SYSBOOT at boot time.
[Question2]
Is it possible to use USB * _DRVVBUS as a GPIO pin when USB * is enabled?
Once USB * is enabled, USB * _DRVVBUS is also wondering if its functionality will be limited to USB.
[Question3]
LCDDATA has 24 bits, but I want to use only 8 bits.
At this time, is it possible to enable the LCD controller and use the unused LCD DATA as GPIO?
Thanks,
Astro