Part Number: J721EXCPXEVM
Other Parts Discussed in Thread: SK-TDA4VM
Hi guys,
I am new to TI development board and I have a little problem. I have followed the guidelines in : https://software-dl.ti.com/jacinto7/esd/processor-sdk-linux-sk-tda4vm/latest/exports/docs/getting_started.html
But when I switch on my sk-tda4vm board with the edge ai sdk and an arducam stereo 1 MP connected via MIPI-CSI2 i have that kind of error at the end :
root@j7-evm:/opt/edge_ai_apps#
U-Boot SPL 2021.01-g15769936a5 (Dec 20 2021 - 17:09:03 +0000)
Model: Texas Instruments J721E SK R5
Board: J721EX-SK rev A
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.9.1--v2021.09a (Terrific Lla')
Trying to boot from MMC2
Starting ATF on ARM64 core...
NOTICE: BL31: v2.5(release):08.01.00.006-dirty
NOTICE: BL31: Built : 16:34:52, Dec 20 2021
U-Boot SPL 2021.01-g15769936a5 (Dec 20 2021 - 16:36:05 +0000)
Model: Texas Instruments J721E SK A72
Board: J721EX-SK rev A
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.9.1--v2021.09a (Terrific Lla')
Trying to boot from MMC2
U-Boot 2021.01-g15769936a5 (Dec 20 2021 - 16:36:05 +0000)
SoC: J721E SR2.0
Model: Texas Instruments J721E SK A72
Board: J721EX-SK rev A
DRAM: 4 GiB
Flash: 0 Bytes
MMC: sdhci@4fb0000: 1
In: serial@2800000
Out: serial@2800000
Err: serial@2800000
Net: am65_cpsw_nuss_slave ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA00101 cpsw_ver: 0x6BA80100 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000
eth1: ethernet@46000000
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc1 is current device
SD/MMC found on device 1
Failed to load 'boot.scr'
483 bytes read in 10 ms (46.9 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc1 ...
Running uenvcmd ...
1 bytes read in 11 ms (0 Bytes/s)
Already setup.
k3_r5f_rproc r5f@41000000: Core 1 is already in use. No rproc commands work
k3_r5f_rproc r5f@41400000: Core 2 is already in use. No rproc commands work
572788 bytes read in 57 ms (9.6 MiB/s)
Load Remote Processor 2 with data@addr=0x82000000 572788 bytes: Success!
301996 bytes read in 35 ms (8.2 MiB/s)
Load Remote Processor 3 with data@addr=0x82000000 301996 bytes: Success!
Failed to load '/lib/firmware/j7-main-r5f1_0-fw'
Failed to load '/lib/firmware/j7-main-r5f1_1-fw'
1436436 bytes read in 83 ms (16.5 MiB/s)
Load Remote Processor 6 with data@addr=0x82000000 1436436 bytes: Success!
1436436 bytes read in 81 ms (16.9 MiB/s)
Load Remote Processor 7 with data@addr=0x82000000 1436436 bytes: Success!
12980288 bytes read in 564 ms (21.9 MiB/s)
Load Remote Processor 8 with data@addr=0x82000000 12980288 bytes: Success!
19270144 bytes read in 818 ms (22.5 MiB/s)
96358 bytes read in 23 ms (4 MiB/s)
10336 bytes read in 19 ms (531.3 KiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
ERROR: reserving fdt memory region failed (addr=fe000000 size=1000000)
ERROR: reserving fdt memory region failed (addr=fc000000 size=2000000)
Loading Device Tree to 000000008fee5000, end 000000008fffffff ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x411fd080]
[ 0.000000] Linux version 5.10.65-gdcc6bedb2c (oe-user@oe-host) (aarch64-none-linux-gnu-gcc (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 9.2.1 20191025, GNU ld (GNU Toolchain1
[ 0.000000] Machine model: Texas Instruments J721E SK
[ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
[ 0.000000] printk: bootconsole [ns16550a0] enabled
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a0000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node vision_apps-r5f-memory@a0100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a1000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a1100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a2000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 31 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a2100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a4000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, size 31 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a4100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a6000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a6000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a6100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a6100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a7000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a7000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a7100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a7100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a8000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c66-dma-memory@a8000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a8100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c66-memory@a8100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a9000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c66-dma-memory@a9000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a9100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c66-memory@a9100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000aa000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c71-dma-memory@aa000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000aa100000, size 79 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c71-memory@aa100000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000b2000000, size 96 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-dma-memory@b2000000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: initialized node vision_apps_shared-memories, compatible id dma-heap-carveout
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000d8000000, size 576 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-core-heap-memory-lo@d8000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000fc000000, size 32 MiB
[ 0.000000] OF: reserved mem: initialized node intercore-eth-r5f-memory@fc000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000fe000000, size 16 MiB
[ 0.000000] OF: reserved mem: initialized node eeprom-shadow-r5f-memory@fe000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000880000000, size 256 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-core-heap-memory-hi@880000000, compatible id shared-dma-pool
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal [mem 0x0000000100000000-0x00000008ffffffff]
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x000000009e7fffff]
[ 0.000000] node 0: [mem 0x000000009e800000-0x00000000aeffffff]
[ 0.000000] node 0: [mem 0x00000000af000000-0x00000000afffffff]
[ 0.000000] node 0: [mem 0x00000000b0000000-0x00000000b7ffffff]
[ 0.000000] node 0: [mem 0x00000000b8000000-0x00000000d7ffffff]
[ 0.000000] node 0: [mem 0x00000000d8000000-0x00000000feffffff]
[ 0.000000] node 0: [mem 0x00000000ff000000-0x00000000ffffffff]
[ 0.000000] node 0: [mem 0x0000000880000000-0x000000088fffffff]
[ 0.000000] node 0: [mem 0x0000000890000000-0x00000008ffffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000008ffffffff]
[ 0.000000] cma: Failed to reserve 512 MiB
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.2
[ 0.000000] percpu: Embedded 2 pages/cpu s49880 r8192 d73000 u131072
[ 0.000000] Detected PIPT I-cache on CPU0
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] CPU features: detected: EL2 vector hardening
[ 0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 65472
[ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),256k(ospi.env),1m(ospi.sysfw),256t
[ 0.000000] Dentry cache hash table entries: 524288 (order: 6, 4194304 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 262144 (order: 5, 2097152 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] software IO TLB: mapped [mem 0x000000009a800000-0x000000009e800000] (64MB)
[ 0.000000] Memory: 2270080K/4194304K available (10880K kernel code, 1346K rwdata, 4288K rodata, 1856K init, 757K bss, 1924224K reserved, 0K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 960 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] GICv3: Distributor has no Range Selector support
[ 0.000000] GICv3: 16 PPIs implemented
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001900000
[ 0.000000] ITS [mem 0x01820000-0x0182ffff]
[ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[ 0.000000] ITS@0x0000000001820000: allocated 1048576 Devices @8a0800000 (flat, esz 8, psz 64K, shr 0)
[ 0.000000] ITS: using cache flushing for cmd queue
[ 0.000000] GICv3: using LPI property table @0x00000008a00b0000
[ 0.000000] GIC: using cache flushing for LPI property table
[ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x00000008a00c0000
[ 0.000000] random: get_random_bytes called from start_kernel+0x31c/0x4c4 with crng_init=0
[ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[ 0.000002] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[ 0.008363] Console: colour dummy device 80x25
[ 0.012926] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[ 0.023595] pid_max: default: 32768 minimum: 301
[ 0.028343] LSM: Security Framework initializing
[ 0.033092] Mount-cache hash table entries: 8192 (order: 0, 65536 bytes, linear)
[ 0.040662] Mountpoint-cache hash table entries: 8192 (order: 0, 65536 bytes, linear)
[ 0.049677] rcu: Hierarchical SRCU implementation.
[ 0.054738] Platform MSI: msi-controller@1820000 domain created
[ 0.060995] PCI/MSI: /bus@100000/interrupt-controller@1800000/msi-controller@1820000 domain created
[ 0.070293] EFI services will not be available.
[ 0.075060] smp: Bringing up secondary CPUs ...
[ 0.080320] Detected PIPT I-cache on CPU1
[ 0.080344] GICv3: CPU1: found redistributor 1 region 0:0x0000000001920000
[ 0.080355] GICv3: CPU1: using allocated LPI pending table @0x00000008a00d0000
[ 0.080388] CPU1: Booted secondary processor 0x0000000001 [0x411fd080]
[ 0.080444] smp: Brought up 1 node, 2 CPUs
[ 0.109790] SMP: Total of 2 processors activated.
[ 0.114595] CPU features: detected: 32-bit EL0 Support
[ 0.119848] CPU features: detected: CRC32 instructions
[ 0.133651] CPU: All CPU(s) started at EL2
[ 0.137847] alternatives: patching kernel code
[ 0.142871] devtmpfs: initialized
[ 0.151176] KASLR disabled due to lack of seed
[ 0.155839] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.165801] futex hash table entries: 512 (order: -1, 32768 bytes, linear)
[ 0.172950] pinctrl core: initialized pinctrl subsystem
[ 0.178511] DMI not present or invalid.
[ 0.182725] NET: Registered protocol family 16
[ 0.187504] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
[ 0.194838] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.202807] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.211085] thermal_sys: Registered thermal governor 'step_wise'
[ 0.211088] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.217492] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.231122] ASID allocator initialised with 65536 entries
[ 0.251760] HugeTLB registered 16.0 GiB page size, pre-allocated 0 pages
[ 0.258615] HugeTLB registered 512 MiB page size, pre-allocated 0 pages
[ 0.265373] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.273146] cryptd: max_cpu_qlen set to 1000
[ 0.279137] k3-chipinfo 43000014.chipid: Family:J721E rev:SR2.0 JTAGID[0x1bb6402f] Detected
[ 0.287931] vsys_3v3: supplied by vusb-main5v0
[ 0.292950] iommu: Default domain type: Translated
[ 0.298069] SCSI subsystem initialized
[ 0.302154] mc: Linux media interface: v0.10
[ 0.306523] videodev: Linux video capture interface: v2.00
[ 0.312148] pps_core: LinuxPPS API ver. 1 registered
[ 0.317219] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.326556] PTP clock support registered
[ 0.330574] EDAC MC: Ver: 3.0.0
[ 0.334335] FPGA manager framework
[ 0.337841] Advanced Linux Sound Architecture Driver Initialized.
[ 0.344455] clocksource: Switched to clocksource arch_sys_counter
[ 0.350890] VFS: Disk quotas dquot_6.6.0
[ 0.354940] VFS: Dquot-cache hash table entries: 8192 (order 0, 65536 bytes)
[ 0.364608] Carveout Heap: Exported 512 MiB at 0x00000000b8000000
[ 0.370899] NET: Registered protocol family 2
[ 0.375502] IP idents hash table entries: 65536 (order: 3, 524288 bytes, linear)
[ 0.384108] tcp_listen_portaddr_hash hash table entries: 4096 (order: 0, 65536 bytes, linear)
[ 0.392895] TCP established hash table entries: 32768 (order: 2, 262144 bytes, linear)
[ 0.401094] TCP bind hash table entries: 32768 (order: 3, 524288 bytes, linear)
[ 0.408900] TCP: Hash tables configured (established 32768 bind 32768)
[ 0.415647] UDP hash table entries: 2048 (order: 0, 65536 bytes, linear)
[ 0.422536] UDP-Lite hash table entries: 2048 (order: 0, 65536 bytes, linear)
[ 0.429934] NET: Registered protocol family 1
[ 0.434642] RPC: Registered named UNIX socket transport module.
[ 0.440699] RPC: Registered udp transport module.
[ 0.445512] RPC: Registered tcp transport module.
[ 0.450316] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.456900] PCI: CLS 0 bytes, default 64
[ 0.461239] hw perfevents: enabled with armv8_cortex_a72 PMU driver, 7 counters available
[ 0.471591] Initialise system trusted keyrings
[ 0.476214] workingset: timestamp_bits=46 max_order=16 bucket_order=0
[ 0.484497] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.490695] NFS: Registering the id_resolver key type
[ 0.495881] Key type id_resolver registered
[ 0.500155] Key type id_legacy registered
[ 0.504273] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.511121] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.518764] 9p: Installing v9fs 9p2000 file system support
[ 0.543973] Key type asymmetric registered
[ 0.548159] Asymmetric key parser 'x509' registered
[ 0.553156] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[ 0.560715] io scheduler mq-deadline registered
[ 0.565340] io scheduler kyber registered
[ 0.570561] pinctrl-single 4301c000.pinctrl: 94 pins, size 376
[ 0.576732] pinctrl-single 11c000.pinctrl: 173 pins, size 692
[ 0.585106] k3-ringacc 2b800000.ringacc: Failed to get MSI domain
[ 0.591364] k3-ringacc 3c000000.ringacc: Failed to get MSI domain
[ 0.599126] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 0.607209] arm-smmu-v3 36600000.iommu: ias 48-bit, oas 48-bit (features 0x00001faf)
[ 0.616575] arm-smmu-v3 36600000.iommu: allocated 524288 entries for cmdq
[ 0.626263] arm-smmu-v3 36600000.iommu: allocated 524288 entries for evtq
[ 0.634155] arm-smmu-v3 36600000.iommu: msi_domain absent - falling back to wired irqs
[ 0.647201] brd: module loaded
[ 0.653269] loop: module loaded
[ 0.656821] sysfs: cannot create duplicate filename '/devices/platform/dma_buf_phys'
[ 0.664751] CPU: 1 PID: 1 Comm: swapper/0 Not tainted 5.10.65-gdcc6bedb2c #1
[ 0.671951] Hardware name: Texas Instruments J721E SK (DT)
[ 0.677551] Call trace:
[ 0.680058] dump_backtrace+0x0/0x1a0
[ 0.683794] show_stack+0x18/0x68
[ 0.687176] dump_stack+0xd0/0x12c
[ 0.690646] sysfs_warn_dup+0x60/0x80
[ 0.694381] sysfs_create_dir_ns+0xe0/0xf8
[ 0.698562] kobject_add_internal+0x98/0x288
[ 0.702918] kobject_add+0x94/0x100
[ 0.706480] device_add+0xe0/0x740
[ 0.709951] platform_device_add+0x100/0x238
[ 0.714308] platform_device_register_full+0xcc/0x150
[ 0.719466] dma_buf_phys_init+0x6c/0x9c
[ 0.723467] do_one_initcall+0x54/0x1b8
[ 0.727380] kernel_init_freeable+0x220/0x2a0
[ 0.731827] kernel_init+0x14/0x114
[ 0.735383] ret_from_fork+0x10/0x34
[ 0.739039] kobject_add_internal failed for dma_buf_phys with -EEXIST, don't try to register things with the same name in the same directory.
[ 0.752197] megasas: 07.714.04.00-rc1
[ 0.757150] libphy: Fixed MDIO Bus: probed
[ 0.761772] tun: Universal TUN/TAP device driver, 1.6
[ 0.767176] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[ 0.773583] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 0.779651] sky2: driver version 1.30
[ 0.783880] VFIO - User Level meta-driver version: 0.3
[ 0.789529] i2c /dev entries driver
[ 0.793671] sdhci: Secure Digital Host Controller Interface driver
[ 0.799986] sdhci: Copyright(c) Pierre Ossman
[ 0.804599] sdhci-pltfm: SDHCI platform and OF driver helper
[ 0.810888] ledtrig-cpu: registered to indicate activity on CPUs
[ 0.817197] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 0.824299] optee: probing for conduit method.
[ 0.828854] optee: revision 3.12 (3d47a131)
[ 0.829106] optee: initialized driver
[ 0.838310] NET: Registered protocol family 17
[ 0.842921] 9pnet: Installing 9P2000 support
[ 0.847304] Key type dns_resolver registered
[ 0.851750] Loading compiled-in X.509 certificates
[ 0.860660] k3-ringacc 2b800000.ringacc: Failed to get MSI domain
[ 0.866993] k3-ringacc 3c000000.ringacc: Failed to get MSI domain
[ 0.875051] ti-sci 44083000.dmsc: ABI: 3.1 (firmware rev 0x0015 '21.9.1--v2021.09a (Terrific Lla')
[ 0.904640] random: fast init done
[ 0.930205] omap_i2c 40b00000.i2c: bus 0 rev0.12 at 100 kHz
[ 0.936294] omap_i2c 40b10000.i2c: bus 1 rev0.12 at 100 kHz
[ 0.942343] omap_i2c 42120000.i2c: bus 2 rev0.12 at 100 kHz
[ 0.972610] i2c i2c-3: Added multiplexed i2c bus 4
[ 0.977583] i2c i2c-3: Added multiplexed i2c bus 5
[ 0.982481] pca954x 3-0071: registered 2 multiplexed busses for I2C switch pca9543
[ 0.990237] omap_i2c 2000000.i2c: bus 3 rev0.12 at 400 kHz
[ 0.996298] omap_i2c 2010000.i2c: bus 6 rev0.12 at 100 kHz
[ 1.024608] i2c i2c-7: Added multiplexed i2c bus 8
[ 1.029580] i2c i2c-7: Added multiplexed i2c bus 9
[ 1.034478] pca954x 7-0070: registered 2 multiplexed busses for I2C switch pca9543
[ 1.042233] omap_i2c 2030000.i2c: bus 7 rev0.12 at 400 kHz
[ 1.048649] ti-sci-intr bus@100000:bus@28380000:interrupt-controller2: Interrupt Router 137 domain created
[ 1.058623] ti-sci-intr bus@100000:interrupt-controller0: Interrupt Router 131 domain created
[ 1.067434] ti-sci-intr bus@100000:main-navss:interrupt-controller1: Interrupt Router 213 domain created
[ 1.077284] ti-sci-inta 33d00000.interrupt-controller: Interrupt Aggregator domain 209 created
[ 1.098359] cdns-torrent-phy 5050000.serdes: 4 lanes, max bit rate 5.400 Gbps
[ 1.106066] j721e-pcie 2900000.pcie: host bridge /bus@100000/pcie@2900000 ranges:
[ 1.113737] j721e-pcie 2900000.pcie: IO 0x0010001000..0x0010010fff -> 0x0010001000
[ 1.122015] j721e-pcie 2900000.pcie: MEM 0x0010011000..0x0017ffffff -> 0x0010011000
[ 1.130292] j721e-pcie 2900000.pcie: IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
[ 1.139184] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
[ 1.146867] j721e-pcie 2910000.pcie: IO 0x0018001000..0x0018010fff -> 0x0018001000
[ 1.155142] j721e-pcie 2910000.pcie: MEM 0x0018011000..0x001fffffff -> 0x0018011000
[ 1.163418] j721e-pcie 2910000.pcie: IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
[ 1.172615] k3-ringacc 2b800000.ringacc: Ring Accelerator probed rings:286, gp-rings[96,20] sci-dev-id:235
[ 1.182488] k3-ringacc 2b800000.ringacc: dma-ring-reset-quirk: disabled
[ 1.189247] k3-ringacc 2b800000.ringacc: RA Proxy rev. 66346100, num_proxies:64
[ 1.198261] k3-ringacc 3c000000.ringacc: Ring Accelerator probed rings:1024, gp-rings[440,150] sci-dev-id:211
[ 1.208417] k3-ringacc 3c000000.ringacc: dma-ring-reset-quirk: disabled
[ 1.215175] k3-ringacc 3c000000.ringacc: RA Proxy rev. 66346100, num_proxies:64
[ 1.223139] 40a00000.serial: ttyS1 at MMIO 0x40a00000 (irq = 15, base_baud = 6000000) is a 8250
[ 1.232549] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 27, base_baud = 3000000) is a 8250
[ 1.241290] printk: console [ttyS2] enabled
[ 1.241290] printk: console [ttyS2] enabled
[ 1.249726] printk: bootconsole [ns16550a0] disabled
[ 1.249726] printk: bootconsole [ns16550a0] disabled
[ 1.260208] 2810000.serial: ttyS3 at MMIO 0x2810000 (irq = 28, base_baud = 3000000) is a 8250
[ 1.269149] 2840000.serial: ttyS6 at MMIO 0x2840000 (irq = 29, base_baud = 3000000) is a 8250
[ 1.320462] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 1.328109] libphy: 46000f00.mdio: probed
[ 1.333459] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867
[ 1.341761] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00101, cpsw version 0x6BA80100 Ports: 2 quirks:00000000
[ 1.355768] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010a, freq:200000000, add_val:4 pps:0
[ 1.370132] vdd_mmc1: supplied by vsys_3v3
[ 1.374989] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fc7100
[ 1.381864] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fc7100
[ 1.388706] omap-mailbox 31f82000.mailbox: omap mailbox rev 0x66fc7100
[ 1.395530] omap-mailbox 31f83000.mailbox: omap mailbox rev 0x66fc7100
[ 1.402332] omap-mailbox 31f84000.mailbox: omap mailbox rev 0x66fc7100
[ 1.411889] j721e-pcie 2900000.pcie: host bridge /bus@100000/pcie@2900000 ranges:
[ 1.419396] j721e-pcie 2900000.pcie: IO 0x0010001000..0x0010010fff -> 0x0010001000
[ 1.427479] j721e-pcie 2900000.pcie: MEM 0x0010011000..0x0017ffffff -> 0x0010011000
[ 1.435557] j721e-pcie 2900000.pcie: IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
[ 2.444841] j721e-pcie 2900000.pcie: PCI host bridge to bus 0000:00
[ 2.451099] pci_bus 0000:00: root bus resource [bus 00-0f]
[ 2.456571] pci_bus 0000:00: root bus resource [io 0x0000-0xffff] (bus address [0x10001000-0x10010fff])
[ 2.466030] pci_bus 0000:00: root bus resource [mem 0x10011000-0x17ffffff]
[ 2.472911] pci 0000:00:00.0: [104c:b00d] type 01 class 0x060400
[ 2.478904] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x4 may corrupt adjacent RW1C bits
[ 2.488536] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x4 may corrupt adjacent RW1C bits
[ 2.498189] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0xe8 may corrupt adjacent RW1C bits
[ 2.507908] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x3e may corrupt adjacent RW1C bits
[ 2.517637] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x92 may corrupt adjacent RW1C bits
[ 2.527358] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0xb2 may corrupt adjacent RW1C bits
[ 2.537104] pci 0000:00:00.0: supports D1
[ 2.541101] pci 0000:00:00.0: PME# supported from D0 D1 D3hot
[ 2.546833] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x84 may corrupt adjacent RW1C bits
[ 2.558346] pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[ 2.566338] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x3e may corrupt adjacent RW1C bits
[ 2.576057] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x3e may corrupt adjacent RW1C bits
[ 2.585780] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x3e may corrupt adjacent RW1C bits
[ 2.597068] pci_bus 0000:01: busn_res: [bus 01-0f] end is updated to 01
[ 2.603675] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 2.608837] pcieport 0000:00:00.0: PME: Signaling with IRQ 492
[ 2.615131] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
[ 2.622622] j721e-pcie 2910000.pcie: IO 0x0018001000..0x0018010fff -> 0x0018001000
[ 2.630703] j721e-pcie 2910000.pcie: MEM 0x0018011000..0x001fffffff -> 0x0018011000
[ 2.638780] j721e-pcie 2910000.pcie: IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
[ 3.648432] j721e-pcie 2910000.pcie: PCI host bridge to bus 0001:00
[ 3.654689] pci_bus 0001:00: root bus resource [bus 00-0f]
[ 3.660162] pci_bus 0001:00: root bus resource [io 0x10000-0x1ffff] (bus address [0x18001000-0x18010fff])
[ 3.669794] pci_bus 0001:00: root bus resource [mem 0x18011000-0x1fffffff]
[ 3.676670] pci 0001:00:00.0: [104c:b00d] type 01 class 0x060400
[ 3.682723] pci 0001:00:00.0: supports D1
[ 3.686720] pci 0001:00:00.0: PME# supported from D0 D1 D3hot
[ 3.694155] pci 0001:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[ 3.703823] pci_bus 0001:01: busn_res: [bus 01-0f] end is updated to 01
[ 3.710429] pci 0001:00:00.0: PCI bridge to [bus 01]
[ 3.715584] pcieport 0001:00:00.0: PME: Signaling with IRQ 494
[ 3.722272] ti-udma 285c0000.dma-controller: Channels: 26 (tchan: 13, rchan: 13, gp-rflow: 8)
[ 3.732801] ti-udma 31150000.dma-controller: Channels: 122 (tchan: 61, rchan: 61, gp-rflow: 16)
[ 3.747966] spi-nor spi0.0: s28hs512t (65536 Kbytes)
[ 3.752945] 8 cmdlinepart partitions found on MTD device 47040000.spi.0
[ 3.759543] Creating 8 MTD partitions on "47040000.spi.0":
[ 3.765015] 0x000000000000-0x000000080000 : "ospi.tiboot3"
[ 3.771034] 0x000000080000-0x000000280000 : "ospi.tispl"
[ 3.776717] 0x000000280000-0x000000680000 : "ospi.u-boot"
[ 3.782554] 0x000000680000-0x0000006c0000 : "ospi.env"
[ 3.788078] 0x0000006c0000-0x0000007c0000 : "ospi.sysfw"
[ 3.793728] 0x0000007c0000-0x000000800000 : "ospi.env.backup"
[ 3.799889] 0x000000800000-0x000003fc0000 : "ospi.rootfs"
[ 3.805641] 0x000003fc0000-0x000004000000 : "ospi.phypattern"
[ 3.856461] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 3.864108] libphy: 46000f00.mdio: probed
[ 3.869300] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver TI DP83867
[ 3.877593] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA00101, cpsw version 0x6BA80100 Ports: 2 quirks:00000000
[ 3.891253] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48
[ 3.898312] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
[ 3.905523] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
[ 3.911842] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010a, freq:500000000, add_val:1 pps:0
[ 3.922426] mmc0: CQHCI version 5.10
[ 3.925085] debugfs: Directory 'pd:27' with parent 'pm_genpd' already present!
[ 3.933297] debugfs: Directory 'pd:26' with parent 'pm_genpd' already present!
[ 3.941515] debugfs: Directory 'pd:242' with parent 'pm_genpd' already present!
[ 3.948848] debugfs: Directory 'pd:241' with parent 'pm_genpd' already present!
[ 3.956160] debugfs: Directory 'pd:240' with parent 'pm_genpd' already present!
[ 3.963476] debugfs: Directory 'pd:239' with parent 'pm_genpd' already present!
[ 3.981201] ALSA device list:
[ 3.984160] No soundcards found.
[ 4.987486] mmc0: SDHCI controller on 4fb0000.mmc [4fb0000.mmc] using ADMA 64-bit
[ 4.995261] Waiting for root device PARTUUID=4b0ab967-02...
[ 5.034358] mmc0: new high speed SDXC card at address b368
[ 5.040202] mmcblk0: mmc0:b368 NCard 58.2 GiB
[ 5.048564] mmcblk0: p1 p2
[ 8.396797] EXT4-fs (mmcblk0p2): recovery complete
[ 8.502695] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 8.510810] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 8.536838] devtmpfs: mounted
[ 8.540188] Freeing unused kernel memory: 1856K
[ 8.544746] Run /sbin/init as init process
[ 8.874259] systemd[1]: System time before build time, advancing clock.
[ 8.964648] NET: Registered protocol family 10
[ 8.969564] Segment Routing with IPv6
[ 8.996416] systemd[1]: systemd 244.5+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD)
[ 9.018179] systemd[1]: Detected architecture arm64.
Welcome to Arago 2021.09!
[ 9.065303] systemd[1]: Set hostname to <j7-evm>.
[ 9.656403] systemd[1]: /lib/systemd/system/docker.socket:6: ListenStream= references a path below legacy directory /var/run/, updating /var/run/docker.sock �→ /run/docker.sock; please update the uni.
[ 9.744783] random: systemd: uninitialized urandom read (16 bytes read)
[ 9.751503] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.
[ 9.763827] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)
[ 9.773754] systemd[1]: Created slice system-getty.slice.
[ OK ] Created slice system-getty.slice.
[ 9.796530] random: systemd: uninitialized urandom read (16 bytes read)
[ 9.803827] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ 9.824525] random: systemd: uninitialized urandom read (16 bytes read)
[ 9.831652] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 9.852636] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password �…ts to Console Directory Watch.
[ 9.876563] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password R�…uests to Wall Directory Watch.
[ 9.900557] systemd[1]: Reached target Paths.
[ OK ] Reached target Paths.
[ 9.920510] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 9.940505] systemd[1]: Reached target Slices.
[ OK ] Reached target Slices.
[ 9.960504] systemd[1]: Reached target Swap.
[ OK ] Reached target Swap.
[ 9.990791] systemd[1]: Listening on RPCbind Server Activation Socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ 10.012532] systemd[1]: Reached target RPC Port Mapper.
[ OK ] Reached target RPC Port Mapper.
[ 10.034910] systemd[1]: Listening on Process Core Dump Socket.
[ OK ] Listening on Process Core Dump Socket.
[ 10.056634] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ 10.094920] systemd[1]: Condition check resulted in Journal Audit Socket being skipped.
[ 10.103255] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 10.124712] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 10.144793] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 10.168687] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 10.188622] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 10.211684] systemd[1]: Mounting Huge Pages File System...
Mounting Huge Pages File System...
[ 10.235030] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 10.260267] systemd[1]: Mounting Kernel Debug File System...
Mounting Kernel Debug File System...
[ 10.290509] systemd[1]: Mounting Temporary Directory (/tmp)...
Mounting Temporary Directory (/tmp)...
[ 10.311634] systemd[1]: Starting Create list of static device nodes for the current kernel...
Starting Create list of st�…odes for the current kernel...
[ 10.339664] systemd[1]: Starting Start psplash boot splash screen...
Starting Start psplash boot splash screen...
[ 10.363838] systemd[1]: Starting RPC Bind...
Starting RPC Bind...
[ 10.380624] systemd[1]: Condition check resulted in File System Check on Root Device being skipped.
[ 10.393075] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 10.425391] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 10.441654] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 10.463284] systemd[1]: Starting udev Coldplug all Devices...
[ 10.467419] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[ 10.469302] cryptodev: loading out-of-tree module taints kernel.
Starting udev Coldplug all Devices...[ 10.482121] cryptodev: driver 1.10 loaded.
[ 10.502956] systemd[1]: Started RPC Bind.
[ OK ] Started RPC Bind.
[ 10.520875] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Mounted Huge Pages File System.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Mounted Temporary Directory (/tmp).
[ OK ] Started Create list of sta�… nodes for the current kernel.
[FAILED] Failed to start Start psplash boot splash screen.
See 'systemctl status psplash-start.service' for details.
[DEPEND] Dependency failed for Star�…progress communication helper.
[ OK ] Started Load Kernel Modules.
[ OK ] Started Remount Root and Kernel File Systems.
Mounting Kernel Configuration File System...
Starting Flush Journal to Persistent Storage...
[ 10.738431] systemd-journald[160]: Received client request to flush runtime journal.
Starting Apply Kernel Variables...
Starting Create Static Device Nodes in /dev...
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Create Static Device Nodes in /dev.
[ OK ] Reached target Local File Systems (Pre).
Mounting /media/ram...
Mounting /var/volatile...
Starting udev Kernel Device Manager...
[ OK ] Started udev Coldplug all Devices.
[ OK ] Mounted /media/ram.
[ OK ] Mounted /var/volatile.
Starting udev Wait for Complete Device Initialization...
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
[ OK ] Started Create Volatile Files and Directories.
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ OK ] Started udev Kernel Device Manager.
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Time Set.
[ OK ] Reached target System Time Synchronized.
[ 12.732195] CAN device driver interface
[ 13.076535] k3-dsp-rproc 4d80800000.dsp: assigned reserved memory node vision-apps-c66-dma-memory@a9000000
[ 13.133790] k3-dsp-rproc 4d80800000.dsp: configured DSP for IPC-only mode
[ 13.147868] PVR_K: 194: Read BVNC 22.104.208.318 from HW device registers
[ 13.172336] PVR_K: 194: RGX Device registered with BVNC 22.104.208.318
[ 13.180178] [drm] Initialized tidss 1.0.0 20180215 for 4a00000.dss on minor 1
[ 13.200678] remoteproc remoteproc0: 4d80800000.dsp is available
[ 13.219284] img_enc 4200000.video-encoder: vxe_enc_probe: using heap 1 for internal alloc
[ 13.230458] [drm] Initialized pvr 1.13.5776728 20170530 for 4e20000000.gpu on minor 0
[ 13.250374] img_dec 4300000.video-decoder: decoder registered as /dev/video0
[ 13.280570] remoteproc remoteproc0: attaching to 4d80800000.dsp
[ 13.280753] k3-dsp-rproc 4d80800000.dsp: DSP initialized in IPC-only mode
[ 13.280762] remoteproc0#vdev0buffer: assigned reserved memory node vision-apps-c66-dma-memory@a9000000
[ 13.281089] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 13.281126] remoteproc0#vdev0buffer: registered virtio0 (type 7)
[ 13.281129] remoteproc remoteproc0: remote processor 4d80800000.dsp is now attached
[ 13.285194] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xd
[ 13.288213] Console: switching to colour frame buffer device 240x67
[ 13.288738] k3-dsp-rproc 4d81800000.dsp: assigned reserved memory node vision-apps-c66-dma-memory@a8000000
[ 13.289887] k3-dsp-rproc 4d81800000.dsp: configured DSP for IPC-only mode
[ 13.289955] remoteproc remoteproc1: 4d81800000.dsp is available
[ 13.290005] remoteproc remoteproc1: attaching to 4d81800000.dsp
[ 13.290105] k3-dsp-rproc 4d81800000.dsp: DSP initialized in IPC-only mode
[ 13.290113] remoteproc1#vdev0buffer: assigned reserved memory node vision-apps-c66-dma-memory@a8000000
[ 13.290424] virtio_rpmsg_bus virtio1: rpmsg host is online
[ 13.290470] remoteproc1#vdev0buffer: registered virtio1 (type 7)
[ 13.290473] remoteproc remoteproc1: remote processor 4d81800000.dsp is now attached
[ 13.290913] k3-dsp-rproc 64800000.dsp: assigned reserved memory node vision-apps-c71-dma-memory@aa000000
[ 13.291930] k3-dsp-rproc 64800000.dsp: configured DSP for IPC-only mode
[ 13.291979] remoteproc remoteproc2: 64800000.dsp is available
[ 13.292027] remoteproc remoteproc2: attaching to 64800000.dsp
[ 13.292059] remoteproc remoteproc2: unsupported resource 65538
[ 13.292173] k3-dsp-rproc 64800000.dsp: DSP initialized in IPC-only mode
[ 13.292243] remoteproc2#vdev0buffer: assigned reserved memory node vision-apps-c71-dma-memory@aa000000
[ 13.295323] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0xd
[ 13.296047] img_enc 4200000.video-encoder: encoder registered as /dev/video1
[ 13.296671] virtio_rpmsg_bus virtio2: rpmsg host is online
[ 13.296709] remoteproc2#vdev0buffer: registered virtio2 (type 7)
[ 13.296713] remoteproc remoteproc2: remote processor 64800000.dsp is now attached
[ 13.298874] virtio_rpmsg_bus virtio2: creating channel rpmsg_chrdev addr 0xd
[ 13.503939] platform 41000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1)
[ 13.509165] platform 41000000.r5f: configured R5F for IPC-only mode
[ 13.510864] tidss 4a00000.dss: [drm] fb0: tidssdrmfb frame buffer device
[ 13.591772] platform 41000000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a0000000
[ 13.601117] remoteproc remoteproc3: 41000000.r5f is available
[ 13.607493] remoteproc remoteproc3: attaching to 41000000.r5f
[ 13.733223] platform 41000000.r5f: R5F core initialized in IPC-only mode
[ 13.814675] remoteproc3#vdev0buffer: assigned reserved memory node vision-apps-r5f-dma-memory@a0000000
[ 13.852862] virtio_rpmsg_bus virtio3: rpmsg host is online
[ 13.867911] remoteproc3#vdev0buffer: registered virtio3 (type 7)
[ 13.889467] virtio_rpmsg_bus virtio3: creating channel ti.ipc4.ping-pong addr 0xd
[ 13.898136] virtio_rpmsg_bus virtio3: creating channel rpmsg_chrdev addr 0xe
[ 13.913139] remoteproc remoteproc3: remote processor 41000000.r5f is now attached
[ 13.948860] platform 5c00000.r5f: configured R5F for IPC-only mode
[ 14.016565] platform 5c00000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a2000000
[ 14.100880] remoteproc remoteproc4: 5c00000.r5f is available
[ 14.171263] remoteproc remoteproc4: attaching to 5c00000.r5f
[ 14.225966] platform 5c00000.r5f: R5F core initialized in IPC-only mode
[ 14.306240] remoteproc4#vdev0buffer: assigned reserved memory node vision-apps-r5f-dma-memory@a2000000
[ 14.333521] virtio_rpmsg_bus virtio4: rpmsg host is online
[ 14.348376] virtio_rpmsg_bus virtio4: creating channel rpmsg_chrdev addr 0xd
[ 14.357467] remoteproc4#vdev0buffer: registered virtio4 (type 7)
[ 14.381643] remoteproc remoteproc4: remote processor 5c00000.r5f is now attached
[ 14.420712] platform 5d00000.r5f: configured R5F for IPC-only mode
[ 14.440939] platform 5d00000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a4000000
[ 14.464934] remoteproc remoteproc5: 5d00000.r5f is available
[ 14.484548] remoteproc remoteproc5: attaching to 5d00000.r5f
[ 14.520255] platform 5d00000.r5f: R5F core initialized in IPC-only mode
[ 14.557726] m_can_platform 40528000.can: m_can device registered (irq=20, version=32)
[ 14.573274] m_can_platform 2701000.can: m_can device registered (irq=42, version=32)
[ 14.589123] m_can_platform 2751000.can: m_can device registered (irq=44, version=32)
[ 14.605446] m_can_platform 2791000.can: m_can device registered (irq=46, version=32)
[ OK ] Created slice system-systemd\x2dfsck.slice.
[ 14.652486] random: crng init done
[ 14.655888] random: 7 urandom warning(s) missed due to ratelimiting
[ 14.680932] remoteproc5#vdev0buffer: assigned reserved memory node vision-apps-r5f-dma-memory@a4000000
[ 14.690709] virtio_rpmsg_bus virtio5: rpmsg host is online
[ 14.696269] remoteproc5#vdev0buffer: registered virtio5 (type 7)
[ 14.702419] remoteproc remoteproc5: remote processor 5d00000.r5f is now attached
[ 14.709919] virtio_rpmsg_bus virtio2: creating channel rpmsg_chrdev addr 0x15
[ 14.719188] virtio_rpmsg_bus virtio2: creating channel ti.ipc4.ping-pong addr 0xe
[ 14.727383] virtio_rpmsg_bus virtio4: creating channel rpmsg_chrdev addr 0x15
[ 14.736577] virtio_rpmsg_bus virtio5: creating channel rpmsg_chrdev addr 0xd
[ 14.744601] virtio_rpmsg_bus virtio5: creating channel rpmsg_chrdev addr 0x15
[ 14.755313] platform 5e00000.r5f: configured R5F for remoteproc mode
[ 14.763990] virtio_rpmsg_bus virtio5: creating channel ti.ipc4.ping-pong addr 0xe
[ 14.771551] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0x15
[ 14.778791] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xe
[ 14.786318] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0x15
[ 14.795320] virtio_rpmsg_bus virtio1: creating channel ti.ipc4.ping-pong addr 0xe
[ 14.805194] virtio_rpmsg_bus virtio4: creating channel ti.ipc4.ping-pong addr 0xe
[ 14.806143] platform 5e00000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a6000000
[ 14.920791] remoteproc remoteproc6: 5e00000.r5f is available
[ 14.930787] remoteproc remoteproc6: Direct firmware load for j7-main-r5f1_0-fw failed with error -2
[ 14.941502] platform 5f00000.r5f: configured R5F for remoteproc mode
[ 14.942422] remoteproc remoteproc6: powering up 5e00000.r5f
[ 14.955928] remoteproc remoteproc6: Direct firmware load for j7-main-r5f1_0-fw failed with error -2
[ 14.970329] remoteproc remoteproc6: request_firmware failed: -2
[ 14.980155] platform 5f00000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a7000000
[ 15.011912] remoteproc remoteproc7: 5f00000.r5f is available
[ 15.017718] remoteproc remoteproc7: Direct firmware load for j7-main-r5f1_1-fw failed with error -2
[ 15.030969] remoteproc remoteproc7: powering up 5f00000.r5f
[ 15.036603] remoteproc remoteproc7: Direct firmware load for j7-main-r5f1_1-fw failed with error -2
[ 15.045662] remoteproc remoteproc7: request_firmware failed: -2
[ OK ] Found device /dev/mmcblk0p1.
Starting File System Check on /dev/mmcblk0p1...
[ OK ] Started File System Check on /dev/mmcblk0p1.
[ 15.472394] remoteproc remoteproc8: b034000.pru is available
Mounting /run/media/mmcblk0p1...
[ 15.489230] remoteproc remoteproc9: b004000.rtu is available
[ 15.497177] remoteproc remoteproc10: b00a000.txpru is available
[ 15.516828] remoteproc remoteproc11: b038000.pru is available
[ 15.524764] remoteproc remoteproc12: b006000.rtu is available
[ 15.533684] remoteproc remoteproc13: b00c000.txpru is available
[ 15.540704] remoteproc remoteproc14: b134000.pru is available
[ 15.548956] remoteproc remoteproc15: b104000.rtu is available
[ 15.555666] remoteproc remoteproc16: b10a000.txpru is available
[ 15.576040] remoteproc remoteproc17: b138000.pru is available
[ 15.590305] usbcore: registered new interface driver usbfs
[ 15.595991] usbcore: registered new interface driver hub
[ 15.602013] remoteproc remoteproc18: b106000.rtu is available
[ 15.609112] usbcore: registered new device driver usb
[ 15.614727] remoteproc remoteproc19: b10c000.txpru is available
[ OK ] Created slice system-weston.slice.
[ 15.684781] omap_rng 4e10000.rng: Random Number Generator ver. 241b34c
Starting Start psplash boot splash screen...
[ OK ] Started Start psplash boot splash screen.
[ OK ] Started Start psplash-syst�…progress communication helper.
[ 15.767017] cdns-csi2rx: probe of 4504000.csi-bridge failed with error -22
[ 15.794143] cdns-csi2rx: probe of 4514000.csi-bridge failed with error -22
[ 15.837060] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ OK ] Mounted /run/media/mmcblk0p1.
[ 16.514012] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 16.519530] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[ 16.527631] xhci-hcd xhci-hcd.0.auto: hcc params 0x200073c9 hci version 0x100 quirks 0x0000002000010010
[ 16.537053] xhci-hcd xhci-hcd.0.auto: irq 648, io mem 0x06410000
[ 16.543220] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10
[ 16.551486] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 16.558728] usb usb1: Product: xHCI Host Controller
[ 16.563601] usb usb1: Manufacturer: Linux 5.10.65-gdcc6bedb2c xhci-hcd
[ 16.570133] usb usb1: SerialNumber: xhci-hcd.0.auto
[ 16.575259] hub 1-0:1.0: USB hub found
[ 16.579039] hub 1-0:1.0: 1 port detected
[ 16.583160] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 16.588645] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
[ 16.596300] xhci-hcd xhci-hcd.0.auto: Host supports USB 3.0 SuperSpeed
[ 16.602867] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 16.611001] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 5.10
[ 16.619260] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 16.626469] usb usb2: Product: xHCI Host Controller
[ 16.631335] usb usb2: Manufacturer: Linux 5.10.65-gdcc6bedb2c xhci-hcd
[ 16.637869] usb usb2: SerialNumber: xhci-hcd.0.auto
[ 16.642963] hub 2-0:1.0: USB hub found
[ 16.646725] hub 2-0:1.0: 1 port detected
[ 17.116470] usb 1-1: new high-speed USB device number 2 using xhci-hcd
[ 17.268778] usb 1-1: New USB device found, idVendor=0451, idProduct=8142, bcdDevice= 1.00
[ 17.276942] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=1
[ 17.284065] usb 1-1: SerialNumber: 32020071A4CD
[ 17.289358] hub 1-1:1.0: USB hub found
[ 17.293136] hub 1-1:1.0: 4 ports detected
[ OK ] Started udev Wait for Complete Device Initialization.
[ 17.396536] usb 2-1: new SuperSpeed Gen 1 USB device number 2 using xhci-hcd
[ OK ] Started Hardware RNG Entropy Gatherer Daemon.
[ 17.420735] usb 2-1: New USB device found, idVendor=0451, idProduct=8140, bcdDevice= 1.00
[ 17.428923] usb 2-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 17.442471] hub 2-1:1.0: USB hub found
[ OK ] Reached target System Initializatio[ 17.449984] hub 2-1:1.0: 4 ports detected
n.
[ OK ] Started Daily rotation of log files.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Timers.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on D-Bus System Message Bus Socket.
Starting Docker Socket for the API.
[ OK ] Listening on dropbear.socket.
Starting Reboot and dump vmcore via kexec...
[ OK ] Listening on Docker Socket for the API.
[ OK ] Started Reboot and dump vmcore via kexec.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
[ OK ] Started Job spooling tools.
[ OK ] Started Periodic Command Scheduler.
[ OK ] Started D-Bus System Message Bus.
Starting Print notice about GPLv3 packages...
Starting IPv6 Packet Filtering Framework...
Starting IPv4 Packet Filtering Framework...
[ OK ] Started irqbalance daemon.
Starting Telephony service...
Starting rc.pvr.service...
Starting startwlan...
Starting Login Service...
Starting Update weston ini�… based on the platform name...
[ 18.006777] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ OK ] Started IPv6 Packet Filtering Framework.
[ OK ] Started IPv4 Packet Filtering Framework.
[ OK ] Started rc.pvr.service.
[ OK ] Started Update weston ini �…ge based on the platform name.
[ OK ] Started Telephony service.
[ OK ] Reached target Network (Pre).
[ OK ] Listening on Load/Save RF �…itch Status /dev/rfkill Watch.
Starting Network Se[ 18.070436] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
rvice...
Starting weston.service...
[ OK ] Started Login Service.
[ 18.144146] Bluetooth: Core ver 2.22
[ 18.152553] NET: Registered protocol family 31
[ 18.157090] Bluetooth: HCI device and connection manager initialized
[ 18.163521] Bluetooth: HCI socket layer initialized
[ 18.172472] Bluetooth: L2CAP socket layer initialized
[ 18.177530] Bluetooth: SCO socket layer initialized
[ 18.256056] Intel(R) Wireless WiFi driver for Linux
[ OK ] Started Network Service.
Starting Wait for Network to be Configured...
Starting Network Name Resolution...
[ 18.388306] TI DP83867 46000f00.mdio:00: attached PHY driver [TI DP83867] (mii_bus:phy_addr=46000f00.mdio:00, irq=POLL)
[ 18.415073] am65-cpsw-nuss 46000000.ethernet eth0: Link is Down
[ OK ] Started Network Name Resolution.
[ OK ] Reached target Network.
[ OK ] Reached target Host and Network Name Lookups.
Starting Avahi mDNS/DNS-SD Stack...
Starting Enable and configure wl18xx bluetooth stack...
[ OK ] Started NFS status monitor for NFSv2/3 locking..
Starting Simple Network Ma�…ent Protocol (SNMP) Daemon....
Starting Permit User Sessions...
[ OK ] Started Enable and configure wl18xx bluetooth stack.
[ OK ] Started Permit User Sessions.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyS2.
[ OK ] Started Serial Getty on ttyS3.
[ OK ] Reached target Login Prompts.
Starting Synchronize System and HW clocks...
Starting Weston Wayland Compositor...
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[FAILED] Failed to start Synchronize System and HW clocks.
See 'systemctl status sync-clocks.service' for details.
[ OK ] Created slice User Slice of UID 0.
Starting User Runtime Directory /run/user/0...
[ OK ] Started User Runtime Directory /run/user/0.
Starting User Manager for UID 0...
[ 19.462815] startwlan.sh[811]: Starting WLAN AP setup
[ 19.480941] startwlan.sh[893]: Starting WLAN AP se
[ 19.481351] startwlan.sh[894]: Starting WLAN AP se
[ 19.577089] startwlan.sh[894]: ddin
[ 19.577527] startwlan.sh[897]: ddin
[ OK ] Started User Manager for UID 0.
[ OK ] Started Session c1 of user root.
[ 19.923088] startwlan.sh[897]: ommand failed: No such file or directory (
[ 19.964121] startwlan.sh[898]: ommand failed: No such file or directory (
[ 20.060208] startwlan.sh[898]: onfiguratioCould not read interface wlp1s0 flags: No such device
[ 20.060468] startwlan.sh[898]: nl80211: Driver does not support authentication/association or connect commands
[ 20.060537] startwlan.sh[898]: nl80211: deinit ifname=wlp1s0 disabled_11b_rates=0
[ 20.092192] startwlan.sh[898]: Could not read interface wlp1s0 flags: No such device
[ 20.092388] startwlan.sh[898]: nl80211 driver initialization failed.
[ 20.092466] startwlan.sh[898]: wlp1s0: interface state UNINITIALIZED->DISABLED
[ 20.092526] startwlan.sh[898]: wlp1s0: AP-DISABLED
[ 20.092585] startwlan.sh[898]: wlp1s0: CTRL-EVENT-TERMINATING
[ 20.092645] startwlan.sh[898]: hostapd_free_hapd_data: Interface wlp1s0 wasn't started
[ 20.844661] startwlan.sh[911]: SIOCSIFADDR: No such device
[ 20.872249] startwlan.sh[911]: wlp1s0: ERROR while getting interface flags: No such device
[ 20.896245] startwlan.sh[911]: SIOCSIFNETMASK: No such device
[ 20.920196] startwlan.sh[911]: wlp1s0: ERROR while getting interface flags: No such device
[ OK ] Started weston.service.
Starting DEMO...
Starting telnetd.service...
[ OK ] Started DEMO.
[ OK ] Started telnetd.service.
[ 22.937390] PVR_K: 868: RGX Firmware image 'rgx.fw.22.104.208.318' loaded
[ 22.944253] PVR_K: 941: RGX Firmware image 'rgx.fw.22.104.208.318' loaded
[ 22.960844] PVR_K:(Fatal): 941: Debug assertion failed! [737]
[ 22.966840] ------------[ cut here ]------------
[ 22.971503] WARNING: CPU: 1 PID: 941 at /jenkins/psdkla-dunfell/release/j7-evm/yocto/tisdk/build/arago-tmp-external-arm-glibc/work/j7_evm-linux/ti-img-rogue-driver/1.13.5776728-r0b/git/binary_j721e_l]
[ 23.000024] Modules linked in: nf_defrag_ipv6 nf_defrag_ipv4 libcrc32c ip_tables x_tables iwlmvm iwlwifi mac80211 bluetooth ecdh_generic ecc cfg80211 rfkill libarc4 xhci_plat_hcd xhci_hcd rpmsg_char 6
[ 23.062784] CPU: 1 PID: 941 Comm: weston Tainted: G O 5.10.65-gdcc6bedb2c #1
[ 23.071112] Hardware name: Texas Instruments J721E SK (DT)
[ 23.076581] pstate: 40000005 (nZcv daif -PAN -UAO -TCO BTYPE=--)
[ 23.082611] pc : PVRSRVRegisterPowerDevice+0xe8/0x1a8 [pvrsrvkm]
[ 23.088632] lr : PVRSRVRegisterPowerDevice+0xe8/0x1a8 [pvrsrvkm]
[ 23.094619] sp : ffff8001200ef730
[ 23.097919] x29: ffff8001200ef730 x28: ffff000824012000
[ 23.103216] x27: 0000000000000001 x26: 0000000000000000
[ 23.108513] x25: ffff8000092700c8 x24: ffff800009270368
[ 23.113807] x23: 0000000000000000 x22: 0000000000000000
[ 23.119102] x21: ffff8000092704e0 x20: ffff800009270560
[ 23.124399] x19: ffff800009270b70 x18: 0000000000000010
[ 23.129695] x17: 0000000000000000 x16: 0000000000000000
[ 23.134992] x15: ffff000820358330 x14: 0000000000000263
[ 23.140288] x13: ffff000820358330 x12: 00000000ffffffea
[ 23.145584] x11: ffff8000111da360 x10: ffff8000111c2320
[ 23.150880] x9 : ffff8000111c2378 x8 : 0000000000017fe8
[ 23.156176] x7 : c0000000ffffefff x6 : 0000000000000001
[ 23.161471] x5 : 0000000000000000 x4 : ffff00087fa81ab0
[ 23.166767] x3 : ffff00087fa889b8 x2 : 0000000000000000
[ 23.172062] x1 : 363f39cd28797600 x0 : 0000000000000000
[ 23.177358] Call trace:
[ 23.179834] PVRSRVRegisterPowerDevice+0xe8/0x1a8 [pvrsrvkm]
[ 23.185507] RGXInitDevPart2+0x234/0x6a0 [pvrsrvkm]
[ 23.190399] RGXInit+0x474/0x5d8 [pvrsrvkm]
[ 23.194597] PVRSRVCommonDeviceInitialise+0x88/0x328 [pvrsrvkm]
[ 23.200528] PVRSRVDeviceOpen+0x98/0x150 [pvrsrvkm]
[ 23.205420] pvr_drm_open+0x44/0x98 [pvrsrvkm]
[ 23.209856] drm_file_alloc+0x144/0x230
[ 23.213677] drm_open+0x14c/0x290
[ 23.216978] drm_stub_open+0xa8/0x160
[ 23.220628] chrdev_open+0xa4/0x1a0
[ 23.224103] do_dentry_open+0x12c/0x398
[ 23.227923] vfs_open+0x2c/0x38
[ 23.231052] path_openat+0x818/0xca8
[ 23.234612] do_filp_open+0x78/0x100
[ 23.238174] do_sys_openat2+0x1f0/0x2a0
[ 23.241994] do_sys_open+0x58/0xa0
[ 23.245381] __arm64_sys_openat+0x24/0x30
[ 23.249378] el0_svc_common.constprop.0+0x78/0x1c8
[ 23.254152] do_el0_svc+0x24/0x90
[ 23.257454] el0_svc+0x14/0x20
[ 23.260494] el0_sync_handler+0xb0/0xb8
[ 23.264316] el0_sync+0x180/0x1c0
[ 23.267617] ---[ end trace d9ac31e2e15f67de ]---
[ 23.773373] PVR_K:(Error): 868: PollForValueKM: Timeout. Expected 0x1 but found 0x0 (mask 0xffffffff). [3145]
[ 23.784487] genirq: Flags mismatch irq 41. 00000004 (pvrsrvkm) vs. 00000004 (pvrsrvkm)
[ 23.792429] PVR_K:(Error): 868: PVRSRVPollForValueKM: Failed! Error(PVRSRV_ERROR_TIMEOUT) CPU linear address(0000000002b33c8c) Expected value(1) [3172]
[ 23.806133] PVR_K:(Error): 941: RGXInit: RGXInitDevPart2 failed (145) [1437]
[ 23.813341] PVR_K: 868: ------------[ PVR DBG: START (High) ]------------
[ 23.820215] PVR_K:(Error): 941: RGXInit() failed (PVRSRV_ERROR_UNABLE_TO_REGISTER_ISR_HANDLER) in PVRSRVCommonDeviceInitialise() [2343]
[ 23.832534] PVR_K: 868: OS kernel info: Linux 5.10.65-gdcc6bedb2c #1 SMP PREEMPT Mon Dec 20 16:38:26 UTC 2021 aarch64
[ 23.843205] PVR_K:(Error): 941: PVRSRVDeviceFinalise() failed (PVRSRV_ERROR_NOT_INITIALISED) in PVRSRVCommonDeviceInitialise() [2352]
[ 23.855459] PVR_K: 868: DDK info: Rogue_DDK_Linux_WS rogueddk 1.13@5776728 (release) j721e_linux
[ 23.864330] PVR_K: 868: Time now: 23864327us
[ 23.868693] PVR_K: 868: Services State: OK
[ 23.872867] PVR_K: 868: Connections: No active connections
[ 23.884492] PVR_K: 868: ------[ Driver Info ]------
[ 23.892496] PVR_K:(Error): 941: PVRSRVDeviceOpen: Failed to initialise device (PVRSRV_ERROR_NOT_INITIALISED) [461]
[ 23.903015] PVR_K: 868: Comparison of UM/KM components: MATCHING
[ 23.909122] PVR_K: 868: KM Arch: 32 Bit
[ 23.913042] PVR_K: 868: UM info: 0.0 @ 0 (debug) build options: 0x00000000
[ 23.928478] PVR_K: 868: KM info: 0.0 @ 0 (debug) build options: 0x00000000
[ 23.940461] PVR_K: 868: Window system: wayland
[ 23.956461] PVR_K: 868: FW info: UNINITIALIZED
[ 23.960998] PVR_K: 868: ------[ RGX Device: Start ]------
[ 23.968484] PVR_K: 868: ------[ RGX Info ]------
[ 23.973191] PVR_K: 868: RGX BVNC: 22.104.208.318 (rogue)
[ 23.988492] PVR_K: 868: RGX Device State: Bad
[ 23.992949] PVR_K: 868: RGX Power State: OFF
[ 24.008464] PVR_K: 868: RGX firmware connection state: DOWN (Fw=offline; OS=ready)
[ 24.016115] PVR_K: 868: RGX FW State: OK (HWRState 0x00000000:)
[ 24.032508] PVR_K: 868: RGX FW Power State: RGXFWIF_POW_OFF (APM disabled: 0 ok, 0 denied, 0 non-idle, 0 retry, 0 other, 0 total. Latency: 100 ms)
[ 24.052477] PVR_K: 868: RGX DVFS: 0 frequency changes. Current frequency: 100.000 MHz (sampled at 23180793645 ns). FW frequency: 100.000 MHz.
[ 24.072461] PVR_K: 868: RGX FW OS 0 - State: offline; Freelists: Not Ok; Priority: 0;
[ 24.088482] PVR_K: 868: Number of HWR: GP(0/0+0), 2D(0/0+0), TA(0/0+0), 3D(0/0+0), CDM(0/0+0), FALSE(0,0,0,0,0)
[ 24.104456] PVR_K: 868: DM 0 (GP)
[ 24.107863] PVR_K: 868: DM 1 (HWRflags 0x00000000: working;)
[ 24.113604] PVR_K: 868: DM 2 (HWRflags 0x00000000: working;)
[ 24.124455] PVR_K: 868: DM 3 (HWRflags 0x00000000: working;)
[ 24.130193] PVR_K: 868: DM 4 (HWRflags 0x00000000: working;)
[ 24.140455] PVR_K: 868: RGX Kernel CCB WO:0x0 RO:0x0
[ 24.145497] PVR_K: 868: RGX Firmware CCB WO:0x0 RO:0x0
[ 24.156454] PVR_K: 868: RGX Kernel CCB commands executed = 0
[ 24.162189] PVR_K: 868: RGX SLR: Forced UFO updates requested = 0
[ 24.172457] PVR_K: 868: FW System config flags = 0x00020020 (Ctx switch options: Medium CSW profile; VDM CS INDEX mode; HWR EN; FBCDCv3.1;)
[ 24.192454] PVR_K: 868: FW OS config flags = 0x00000007 (Ctx switch: TA; 3D; CDM;)
[ 24.200099] PVR_K: 868: (!) RGX power is down. No registers dumped
[ 24.212454] PVR_K: 868: ------[ RGX FW Trace Info ]------
[ 24.217929] PVR_K: 868: Debug log type: none
[ 24.228454] PVR_K: 868: RGX FW thread 0: Trace buffer not yet allocated
[ 24.235143] PVR_K: 868: ------[ Full CCB Status ]------
[ 24.244456] PVR_K: 868: ------[ RGX Device: End ]------
[ 24.249759] PVR_K: 868: ------[ System Summary ]------
[ 24.260454] PVR_K: 868: Device System Power State: ON
[ 24.265582] PVR_K: 868: MaxHWTOut: 500000us, WtTryCt: 10000, WDGTOut(on,off): (10000ms,3600000ms)
[ 24.276466] PVR_K: 868: ------[ Server Thread Summary ]------
[ 24.282291] PVR_K: 868: pvr_defer_free : Running
[ 24.292454] PVR_K: 868: Number of deferred cleanup items : 0
[ 24.298538] PVR_K: 868: pvr_device_wdg : Running
[ 24.308454] PVR_K: 868: pvr_cacheop : Running
[ 24.313070] PVR_K: 868: Configuration: QSZ: 16, UKT: -1, KDFT: 131072, LINESIZE: 64, PGSIZE: 65536, KDF: Yes, URBF: Yes
[ 24.332453] PVR_K: 868: Pending deferred CacheOp entries : 0
[ 24.338542] PVR_K: 868: ------[ AppHint Settings ]------
[ 24.348454] PVR_K: 868: Build Vars
[ 24.352108] PVR_K: 868: HWRDebugDumpLimit: 0x00000001
[ 24.364458] PVR_K: 868: EnableTrustedDeviceAceConfig: N
[ 24.370114] PVR_K: 868: CleanupThreadPriority: 0x00000005
[ 24.380461] PVR_K: 868: WatchdogThreadPriority: 0x00000000
[ 24.386392] PVR_K: 868: HWPerfClientBufferSize: 0x000c0000
[ 24.396453] PVR_K: 868: Module Params
[ 24.400374] PVR_K: 868: none
[ 24.403683] PVR_K: 868: Debugfs Params
[ 24.412456] PVR_K: 868: CacheOpConfig: 0x0000000c
[ 24.417590] PVR_K: 868: CacheOpUMKMThresholdSize: 0xffffffff
[ 24.428455] PVR_K: 868: Debugfs Params Device ID: 0
[ 24.433590] PVR_K: 868: none
[ 24.444468] PVR_K: 868: ------[ HTB Log state: Off ]------
[ 24.450058] PVR_K: 868: ------[ Active Sync Checkpoints ]------
[ 24.456069] ------[ Native Fence Sync: timelines ]------
[ 24.461385] foreign_sync: @0 ctx=3 refs=1
[ 24.465392] PVR_K: 868: ------------[ PVR DBG: END ]------------
[ 24.476519] ------------[ cut here ]------------
[ 24.481184] WARNING: CPU: 1 PID: 868 at /jenkins/psdkla-dunfell/release/j7-evm/yocto/tisdk/build/arago-tmp-external-arm-glibc/work/j7_evm-linux/ti-img-rogue-driver/1.13.5776728-r0b/git/binary_j721e_l]
[ 24.509792] Modules linked in: iptable_nat xt_MASQUERADE nf_nat nf_conntrack nf_defrag_ipv6 nf_defrag_ipv4 libcrc32c ip_tables x_tables iwlmvm iwlwifi mac80211 bluetooth ecdh_generic ecc cfg80211 rfk6
[ 24.576544] CPU: 1 PID: 868 Comm: weston-launch Tainted: G W O 5.10.65-gdcc6bedb2c #1
[ 24.585479] Hardware name: Texas Instruments J721E SK (DT)
[ 24.590948] pstate: 80000005 (Nzcv daif -PAN -UAO -TCO BTYPE=--)
[ 24.596970] pc : PVRSRVDebugRequest+0x498/0x628 [pvrsrvkm]
[ 24.602470] lr : PVRSRVDebugRequest+0x498/0x628 [pvrsrvkm]
[ 24.607937] sp : ffff80001ff8f7f0
[ 24.611237] x29: ffff80001ff8f7f0 x28: ffff800009347000
[ 24.616533] x27: 0000000000000000 x26: ffff8000092b9bd8
[ 24.621829] x25: ffff000822aa6400 x24: 0000000000000009
[ 24.627125] x23: 0000000000000002 x22: 0000000000000000
[ 24.632421] x21: 0000000000000000 x20: ffff000822aa64d8
[ 24.637717] x19: ffff000826745ca0 x18: 0000000000000000
[ 24.643013] x17: 0000000000000000 x16: 0000000000000000
[ 24.648308] x15: 0000a7e30ffebade x14: 000000000000038c
[ 24.653605] x13: 000000000000038c x12: 0000000000000000
[ 24.658901] x11: 0000000000001226 x10: 00000000000009a0
[ 24.664196] x9 : ffff80001ff8f630 x8 : ffff000828152600
[ 24.669492] x7 : ffff00087fa8b140 x6 : ffff00087fa8b0c0
[ 24.674788] x5 : ffff800010e30000 x4 : 000000000000000c
[ 24.680084] x3 : 0000000000000000 x2 : ffffffffffffff00
[ 24.685381] x1 : 0000000000000000 x0 : ffff000826741980
[ 24.690677] Call trace:
[ 24.693144] PVRSRVDebugRequest+0x498/0x628 [pvrsrvkm]
[ 24.698296] PVRSRVPollForValueKM+0x17c/0x180 [pvrsrvkm]
[ 24.703623] RGXPostPowerState+0xd4/0x178 [pvrsrvkm]
[ 24.708601] PVRSRVSetDevicePowerStateKM+0x174/0x2d0 [pvrsrvkm]
[ 24.714533] PVRSRVDeviceFinalise+0xc4/0x458 [pvrsrvkm]
[ 24.719772] PVRSRVCommonDeviceInitialise+0x98/0x328 [pvrsrvkm]
[ 24.725704] PVRSRVDeviceOpen+0x98/0x150 [pvrsrvkm]
[ 24.730596] pvr_drm_open+0x44/0x98 [pvrsrvkm]
[ 24.735031] drm_file_alloc+0x144/0x230
[ 24.738851] drm_open+0x14c/0x290
[ 24.742153] drm_stub_open+0xa8/0x160
[ 24.745803] chrdev_open+0xa4/0x1a0
[ 24.749280] do_dentry_open+0x12c/0x398
[ 24.753100] vfs_open+0x2c/0x38
[ 24.756229] path_openat+0x818/0xca8
[ 24.759790] do_filp_open+0x78/0x100
[ 24.763351] do_sys_openat2+0x1f0/0x2a0
[ 24.767173] do_sys_open+0x58/0xa0
[ 24.770560] __arm64_sys_openat+0x24/0x30
[ 24.774557] el0_svc_common.constprop.0+0x78/0x1c8
[ 24.779331] do_el0_svc+0x24/0x90
[ 24.782633] el0_svc+0x14/0x20
[ 24.785673] el0_sync_handler+0xb0/0xb8
[ 24.789495] el0_sync+0x180/0x1c0
[ 24.792795] ---[ end trace d9ac31e2e15f67df ]---
[ 24.800506] PVR_K:(Error): 868: RGXPostPowerState: Polling for 'FW started' flag failed. [630]
[ 24.812489] PVR_K: 868: BIF0 - OK
[ 24.815883] PVR_K: 868: RGX firmware connection state: DOWN (Fw=offline; OS=ready)
[ 24.830275] PVR_K: 868: RGX FW State: OK (HWRState 0x00000000:)
[ 24.840462] PVR_K: 868: RGX FW Power State: RGXFWIF_POW_OFF (APM disabled: 0 ok, 0 denied, 0 non-idle, 0 retry, 0 other, 0 total. Latency: 100 ms)
[ 24.860457] PVR_K: 868: RGX DVFS: 0 frequency changes. Current frequency: 100.000 MHz (sampled at 23180793645 ns). FW frequency: 100.000 MHz.
[ 24.880455] PVR_K: 868: RGX FW OS 0 - State: offline; Freelists: Not Ok; Priority: 0;
_____ _____ _ _
| _[ 24.892484] PVR_K: 868: Number of HWR: GP(0/0+0), 2D(0/0+0), TA(0/0+0), 3D(0/0+0), CDM(0/0+0), FALSE(0,0,0,0,0)
|___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _[ 24.908466] PVR_K: 868: DM 0 (GP)
| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_[ 24.913733] PVR_K: 868: DM 1 (HWRflags 0x00000000: working;)
|___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org j7-evm ttyS2
Arago 2021.09 j7-evm ttyS2
j7-ev[ 24.936476] PVR_K: 868: DM 2 (HWRflags 0x00000000: working;)
m login: [ 24.839665] startwlan.sh[949]: iperf3: error - unabl[ 24.952454] PVR_K: 868: DM 3 (HWRflags 0x00000000: working;)
e to start listener for connections: Cannot assign requested add[ 24.958726] PVR_K: 868: DM 4 (HWRflags 0x00000000: working;)
ress
[ 24.839804] startwlan.sh[949]: iperf3: exiting
[ 24.976458] PVR_K: 868: ------[ RGX registers ]------
[ 24.984458] PVR_K: 868: RGX Register Base Address (Linear): 0x000000000750eae0
[ 24.996457] PVR_K: 868: RGX Register Base Address (Physical): 0x4E20000000
[ 25.003414] PVR_K: 868: CORE_ID : 0x0000000008470000
[ 25.016453] PVR_K: 868: CORE_REVISION : 0x00D0013E
[ 25.024481] PVR_K: 868: DESIGNER_REV_FIELD1 : 0x00000000
[ 25.030753] PVR_K: 868: DESIGNER_REV_FIELD2 : 0x00000000
[ 25.044464] PVR_K: 868: CHANGESET_NUMBER : 0x0000000000000000
[ 25.051419] PVR_K: 868: CLK_CTRL : 0x0aaaaa002a2aaaaa
[ 25.064454] PVR_K: 868: CLK_STATUS : 0x0000000000600000
[ 25.071409] PVR_K: 868: CLK_CTRL2 : 0x0000000000000000
[ 25.084454] PVR_K: 868: CLK_STATUS2 : 0x0000000000000000
[ 25.091403] PVR_K: 868: EVENT_STATUS : 0x00000600
[ 25.104457] PVR_K: 868: TIMER : 0x000000000216a2cf
[ 25.111406] PVR_K: 868: BIF_FAULT_BANK0_MMU_STATUS : 0x00000000
[ 25.120487] PVR_K: 868: BIF_FAULT_BANK0_REQ_STATUS : 0x0000000000000000
[ 25.128468] PVR_K: 868: BIF_FAULT_BANK1_MMU_STATUS : 0x00000000
[ 25.140461] PVR_K: 868: BIF_FAULT_BANK1_REQ_STATUS : 0x0000000000000000
[ 25.152457] PVR_K: 868: BIF_MMU_STATUS : 0x00000000
[ 25.158716] PVR_K: 868: BIF_MMU_ENTRY : 0x00000000
[ 25.172455] PVR_K: 868: BIF_MMU_ENTRY_STATUS : 0x0000000000000000
[ 25.179409] PVR_K: 868: BIF_STATUS_MMU : 0x00000000
[ 25.192455] PVR_K: 868: BIF_READS_EXT_STATUS : 0x00000000
[ 25.198713] PVR_K: 868: BIF_READS_INT_STATUS : 0x00000000
[ 25.212456] PVR_K: 868: BIFPM_STATUS_MMU : 0x00000000
[ 25.218714] PVR_K: 868: BIFPM_READS_EXT_STATUS : 0x00000000
[ 25.232461] PVR_K: 868: BIFPM_READS_INT_STATUS : 0x00000000
[ 25.238725] PVR_K: 868: Warning: BRN44871 is present
[ 25.252458] PVR_K: 868: BIF_CAT_BASE_INDEX : 0x0000000000000000
[ 25.260466] PVR_K: 868: BIF_CAT_BASE0 : 0x0000000000000000
[ 25.267423] PVR_K: 868: BIF_CAT_BASE1 : 0x0000000000000000
[ 25.280454] PVR_K: 868: BIF_CAT_BASE2 : 0x0000000000000000
[ 25.287407] PVR_K: 868: BIF_CAT_BASE3 : 0x0000000000000000
[ 25.300454] PVR_K: 868: BIF_CAT_BASE4 : 0x0000000000000000
[ 25.307403] PVR_K: 868: BIF_CAT_BASE5 : 0x0000000000000000
[ 25.320457] PVR_K: 868: BIF_CAT_BASE6 : 0x0000000000000000
[ 25.331573] PVR_K: 868: BIF_CAT_BASE7 : 0x0000000000000000
[ 25.338544] PVR_K: 868: BIF_CTRL_INVAL : 0x00000000
[ 25.352462] PVR_K: 868: BIF_CTRL : 0x000000C0
[ 25.358721] PVR_K: 868: BIF_PM_CAT_BASE_VCE0 : 0x0000000000000000
[ 25.372454] PVR_K: 868: BIF_PM_CAT_BASE_TE0 : 0x0000000000000000
[ 25.379403] PVR_K: 868: BIF_PM_CAT_BASE_ALIST0 : 0x0000000000000000
[ 25.392454] PVR_K: 868: BIF_PM_CAT_BASE_VCE1 : 0x0000000000000000
[ 25.399403] PVR_K: 868: BIF_PM_CAT_BASE_TE1 : 0x0000000000000000
[ 25.412466] PVR_K: 868: BIF_PM_CAT_BASE_ALIST1 : 0x0000000000000000
[ 25.420460] PVR_K: 868: PERF_TA_PHASE : 0x00000000
[ 25.432469] PVR_K: 868: PERF_TA_CYCLE : 0x00000000
[ 25.438724] PVR_K: 868: PERF_3D_PHASE : 0x00000000
[ 25.452456] PVR_K: 868: PERF_3D_CYCLE : 0x00000000
[ 25.458715] PVR_K: 868: PERF_TA_OR_3D_CYCLE : 0x00000000
[ 25.472455] PVR_K: 868: PERF_TA_AND_3D_CYCLE : 0x00000000
[ 25.478711] PVR_K: 868: PERF_COMPUTE_PHASE : 0x00000000
[ 25.492455] PVR_K: 868: PERF_COMPUTE_CYCLE : 0x00000000
[ 25.498712] PVR_K: 868: PM_PARTIAL_RENDER_ENABLE : 0x00000000
[ 25.512454] PVR_K: 868: ISP_RENDER : 0x00000000
[ 25.518713] PVR_K: 868: TLA_STATUS : 0x0000000000000000
[ 25.532461] PVR_K: 868: MCU_FENCE : 0x0000000000000000
[ 25.544459] PVR_K: 868: VDM_CONTEXT_STORE_STATUS : 0x00000001
[ 25.550715] PVR_K: 868: VDM_CONTEXT_STORE_TASK0 : 0x0000000000000000
[ 25.560467] PVR_K: 868: VDM_CONTEXT_STORE_TASK1 : 0x0000000000000000
[ 25.567424] PVR_K: 868: VDM_CONTEXT_STORE_TASK2 : 0x0000000000000000
[ 25.580454] PVR_K: 868: VDM_CONTEXT_RESUME_TASK0 : 0x0000000000000000
[ 25.587407] PVR_K: 868: VDM_CONTEXT_RESUME_TASK1 : 0x0000000000000000
[ 25.600455] PVR_K: 868: VDM_CONTEXT_RESUME_TASK2 : 0x0000000000000000
[ 25.607403] PVR_K: 868: ISP_CTL : 0x00000000
[ 25.620454] PVR_K: 868: ISP_STATUS : 0x00000000
[ 25.626708] PVR_K: 868: MTS_INTCTX : 0x00000000
[ 25.635260] PVR_K: 868: MTS_BGCTX : 0x00000000
[ 25.648459] PVR_K: 868: MTS_BGCTX_COUNTED_SCHEDULE : 0x00000000
[ 25.655027] PVR_K: 868: MTS_SCHEDULE : 0x00000000
[ 25.661291] PVR_K: 868: MTS_GPU_INT_STATUS : 0x00000600
[ 25.676456] PVR_K: 868: CDM_CONTEXT_STORE_STATUS : 0x00000000
[ 25.682713] PVR_K: 868: CDM_CONTEXT_PDS0 : 0x0000000000000000
[ 25.696454] PVR_K: 868: CDM_CONTEXT_PDS1 : 0x0000000000000000
[ 25.703408] PVR_K: 868: CDM_TERMINATE_PDS : 0x0000000000000000
[ 25.716454] PVR_K: 868: CDM_TERMINATE_PDS1 : 0x0000000000000000
[ 25.723409] PVR_K: 868: SIDEKICK_IDLE : 0x0000007E
[ 25.736456] PVR_K: 868: SLC_IDLE : 0x000000FF
[ 25.742730] PVR_K: 868: SLC_STATUS0 : 0x00000000
[ 25.748987] PVR_K: 868: SLC_STATUS1 : 0x0000000000000000
[ 25.764459] PVR_K: 868: SLC_STATUS2 : 0x0000000000000000
[ 25.776455] PVR_K: 868: SLC_CTRL_BYPASS : 0x01000000
[ 25.782713] PVR_K: 868: SLC_CTRL_MISC : 0x0000000000200003
[ 25.796460] PVR_K: 868: MIPS_ADDR_REMAP1_CONFIG1 : 0x1FC00001
[ 25.802718] PVR_K: 868: MIPS_ADDR_REMAP1_CONFIG2 : 0x00000008a912f00c
[ 25.816473] PVR_K: 868: MIPS_ADDR_REMAP2_CONFIG1 : 0x1FC01001
[ 25.828456] PVR_K: 868: MIPS_ADDR_REMAP2_CONFIG2 : 0x00000008a913e00c
[ 25.840455] PVR_K: 868: MIPS_ADDR_REMAP3_CONFIG1 : 0x1FC02001
[ 25.846713] PVR_K: 868: MIPS_ADDR_REMAP3_CONFIG2 : 0x00000008a912d00c
[ 25.860456] PVR_K: 868: MIPS_ADDR_REMAP4_CONFIG1 : 0x1FC00000
[ 25.866715] PVR_K: 868: MIPS_ADDR_REMAP4_CONFIG2 : 0x000000000000000c
[ 25.880457] PVR_K: 868: MIPS_ADDR_REMAP5_CONFIG1 : 0x00000001
[ 25.886718] PVR_K: 868: MIPS_ADDR_REMAP5_CONFIG2 : 0x00000008a912f00c
[ 25.900454] PVR_K: 868: MIPS_WRAPPER_CONFIG : 0x000000000001cf80
[ 25.907404] PVR_K: 868: MIPS_EXCEPTION_STATUS : 0x00000022
[ 25.919107] PVR_K: 868: ---- [ MIPS internal state ] ----
[ 25.924587] PVR_K: 868: PC : 0xFFFFFFFF
[ 25.936454] PVR_K: 868: STATUS_REGISTER : 0x00000000
[ 25.942708] PVR_K: 868: CAUSE_REGISTER : 0x00000000
[ 25.952466] PVR_K: 868: Interrupt uses general interrupt vector
[ 25.958811] PVR_K: 868: BAD_REGISTER : 0x00000000
[ 25.972454] PVR_K: 868: EPC : 0xFFFFFFFF
[ 25.978710] PVR_K: 868: SP : 0x00000000
[ 25.991080] PVR_K: 868: BAD_INSTRUCTION : 0x00000000
[ 26.004461] PVR_K: 868: TLB :
[ 26.009770] PVR_K: 868: 0) VA 0x00000000 ( 4k) -> PA0 0x00000000 C, PA1 0x00000000 C
[ 26.024464] PVR_K: 868: 1) VA 0x00000000 ( 4k) -> PA0 0x00000000 C, PA1 0x00000000 C
[ 26.040463] PVR_K: 868: 2) VA 0x00000000 ( 4k) -> PA0 0x00000000 C, PA1 0x00000000 C
[ 26.048979] PVR_K: 868: 3) VA 0x00000000 ( 4k) -> PA0 0x00000000 C, PA1 0x00000000 C
[ 26.064455] PVR_K: 868: 4) VA 0x00000000 ( 4k) -> PA0 0x00000000 C, PA1 0x00000000 C
[ 26.080458] PVR_K: 868: 5) VA 0x00000000 ( 4k) -> PA0 0x00000000 C, PA1 0x00000000 C
[ 26.089367] PVR_K: 868: 6) VA 0x00000000 ( 4k) -> PA0 0x00000000 C, PA1 0x00000000 C
[ 26.104457] PVR_K: 868: 7) VA 0x00000000 ( 4k) -> PA0 0x00000000 C, PA1 0x00000000 C
[ 26.116454] PVR_K: 868: 8) VA 0x00000000 ( 4k) -> PA0 0x00000000 C, PA1 0x00000000 C
[ 26.128457] PVR_K: 868: 9) VA 0x00000000 ( 4k) -> PA0 0x00000000 C, PA1 0x00000000 C
[ 26.140456] PVR_K: 868: 10) VA 0x00000000 ( 4k) -> PA0 0x00000000 C, PA1 0x00000000 C
[ 26.152456] PVR_K: 868: 11) VA 0x00000000 ( 4k) -> PA0 0x00000000 C, PA1 0x00000000 C
[ 26.164456] PVR_K: 868: 12) VA 0x00000000 ( 4k) -> PA0 0x00000000 C, PA1 0x00000000 C
[ 26.176470] PVR_K: 868: 13) VA 0x00000000 ( 4k) -> PA0 0x00000000 C, PA1 0x00000000 C
[ 26.188463] PVR_K: 868: 14) VA 0x00000000 ( 4k) -> PA0 0x00000000 C, PA1 0x00000000 C
[ 26.200462] PVR_K: 868: 15) VA 0x00000000 ( 4k) -> PA0 0x00000000 C, PA1 0x00000000 C
[ 26.212463] PVR_K: 868: --------------------------------
[ 26.224464] PVR_K:(Error): 868: PVRSRVDeviceFinalise: Failed to set device 00000000e9e8fc38 power state to 'on' (PVRSRV_ERROR_TIMEOUT) [2913]
[ 26.244458] PVR_K:(Error): 868: PVRSRVDeviceFinalise() failed (PVRSRV_ERROR_TIMEOUT) in PVRSRVCommonDeviceInitialise() [2352]
[ 26.260459] PVR_K:(Error): 868: PVRSRVDeviceOpen: Failed to initialise device (PVRSRV_ERROR_TIMEOUT) [461]
[ 26.467666] PVR_K:(Error): 905: PVRSRVDeviceOpen: Driver already in bad state. Device open failed. [450]
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPLv3 packages:
autoconf
bash-dev
bash
bc
binutils
cifs-utils
coreutils-stdbuf
coreutils
cpio
cpp-symlinks
cpp
dosfstools
elfutils
g++-symlinks
g++
gawk
gcc-symlinks
gcc
gdb
gdbserver
gettext
glmark2
gstreamer1.0-libav-dev
gstreamer1.0-libav
gzip
less
libasm1
libbfd
libdw1
libelf1
libgdbm-compat4
libgdbm-dev
libgdbm6
libgettextlib
libgettextsrc
libgmp-dev
libgmp10
libgmpxx4
libidn2-0
libidn2-dev
libmpc3
libmpfr6
libreadline-dev
libreadline8
libunistring-dev
libunistring2
m4-dev
m4
make
nettle-dev
nettle
parted
python3-rfc3987
python3-strict-rfc3339
tar
which
zeromq
If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************