This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C5517: problem about VoLIB component AEU

Part Number: TMS320C5517

Hi,

 I am using AEU Automatic Level Control(ALC)  to implement  automatic gain  control in a voice system , when I set ALC target level to -15dBm0(veuConfig.alc_recv_level  = -15), the Rxout  output level not the expected  -15dbm0( I measure the output signal with a level meter).

AEU  seting(veuControl)  is:

80
0
0x0121
0x0121
2
-15
3
-15

input Rxin signal is in  inBufRx and

    veuReceiveIn (veuInst,inBufRx );

       veuSendIn (veuInst, inBufTx, inBufRx, outBufTx, NULL);

  then, the Rxout is in  inBufRx..

when the inBufRx is output from DA, the level should be -15dbm0.

 but the result is the output level varied with the input level changed.

Is there something wrong?

 the Volib version is 2_1_0_1(ti_mas_volib_2_1_0_1_C55_cpu3).

the CCS is Version:5.5.0.00077.

Best Regards!

Dudechao